Other Parts Discussed in Thread: TMS570LS1115
Hi
Im making a board with the TMS570LS1115 and was wondering about some stuff. I need 12 PWMs for 12 different motors and was thinking on using the ePWM1:6 but I saw that the ePWM1A is also the N2HET1_PIN_nDIS and I'm not sure if I can use that pin as PWM output...
Im going to use 24 external interrupts from the encoders of the motors, so Im planning to use the N2HET1 module. So... my question is basically what action that pin does and if I could use that pin as PWM output even when Im using the N2HET module..
And also Im using an ADC sigma delta for some analogic data I need. For this, as Im using the 144 package, I will use the MibSPI1. And here I have one more question. With multi buffered it means I can be sending/receiving data from many sources at the same time??
Best regards!!