Other Parts Discussed in Thread: EK-TM4C123GXL
I am trying to write some UART drivers using the TM4C123GH5PMI based Stellaris Launchpad, and have stumbled upon a bit of confusion with regards to the UARTSysClk frequency referenced in the Baud Rate Generator section of the data sheet. I have seen some of the examples from Valavano's book and class, though the UART.c files that I am using as a guide to understand and build all have different values as assumed UARTSysClk values...
One such example shows:
//------------UART_Init------------
// Wait for new serial port input
// Initialize the UART for 115,200 baud rate (assuming 16 MHz UART clock),
// 8 bit word length, no parity bits, one stop bit, FIFOs enabled
// Input: none
// Output: none
void UART_Init(void){
SYSCTL_RCGC1_R |= SYSCTL_RCGC1_UART0; // activate UART0
SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOA; // activate port A
UART0_CTL_R &= ~UART_CTL_UARTEN; // disable UART
UART0_IBRD_R = 8; // IBRD = int(16,000,000 / (16 * 115,200)) = int(8.68)
UART0_FBRD_R = 43; // FBRD = round(0.68 * 64 ) = 43
// 8 bit word length (no parity bits, one stop bit, FIFOs)
UART0_LCRH_R = (UART_LCRH_WLEN_8|UART_LCRH_FEN);
UART0_CTL_R |= UART_CTL_UARTEN; // enable UART
GPIO_PORTA_AFSEL_R |= 0x03; // enable alt funct on PA1-0
GPIO_PORTA_DEN_R |= 0x03; // enable digital I/O on PA1-0
// configure PA1-0 as UART
GPIO_PORTA_PCTL_R = (GPIO_PORTA_PCTL_R&0xFFFFFF00)+0x00000011;
GPIO_PORTA_AMSEL_R &= ~0x03; // disable analog functionality on PA
}
Yet another shows:
//------------UART_Init------------
// Initialize the UART for 115,200 baud rate (assuming 50 MHz UART clock),
// 8 bit word length, no parity bits, one stop bit, FIFOs enabled
// Input: none
// Output: none
void UART_Init(void){
SYSCTL_RCGC1_R |= SYSCTL_RCGC1_UART0; // activate UART0
SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOA; // activate port A
UART0_CTL_R &= ~UART_CTL_UARTEN; // disable UART
UART0_IBRD_R = 27; // IBRD = int(50,000,000 / (16 * 115,200)) = int(27.1267)
UART0_FBRD_R = 8; // FBRD = int(0.1267 * 64 + 0.5) = 8
// 8 bit word length (no parity bits, one stop bit, FIFOs)
UART0_LCRH_R = (UART_LCRH_WLEN_8|UART_LCRH_FEN);
UART0_CTL_R |= UART_CTL_UARTEN; // enable UART
GPIO_PORTA_AFSEL_R |= 0x03; // enable alt funct on PA1-0
GPIO_PORTA_DEN_R |= 0x03; // enable digital I/O on PA1-0
// configure PA1-0 as UART
GPIO_PORTA_PCTL_R = (GPIO_PORTA_PCTL_R&0xFFFFFF00)+0x00000011;
GPIO_PORTA_AMSEL_R &= ~0x03; // disable analog functionality on PA
}
and looking through the datasheet, I would have guess that it would be a value of 80 MHz upon reset...