This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Delay Calculation

Hello,

I have a Stellaris Launchpad LM4F120XL, I am having troubles calculating delays. I set the System Clock to 20MHz with the following code "SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);". Now I want a 1 second delay, what is the formula I use to be able to calculate the correct number to pass as a parameter to the SysCtlDelay() function so it can give me a 1 seccond delay.

Thank You