This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

timers and ADC

Hai 

I want to updates the ADC values for every 5 min.

I written the code here

please help me it is not executed where i did wrong in this.

int
main(void)
{

int bb;
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPUEnable();

ROM_FPULazyStackingEnable();

/

/*Uart functions............................................................*/

SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

lcd_init();
SysCtlDelay(SysCtlClockGet() / 12);
lcdstr(0x80,(unsigned char *)"Remote Monitoring");
SysCtlDelay(100000);
lcdstr(0x80," ");

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG); //For LED

ROM_GPIOPinTypeGPIOOutput(GPIO_PORTG_BASE, GPIO_PIN_2); //pin as output

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

GPIOPinConfigure(GPIO_PA0_U0RX);

GPIOPinConfigure(GPIO_PA1_U0TX);

ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));

UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);

// UARTStdioConfig(0, 115200, 16000000);

UARTFIFOEnable(UART0_BASE);

UARTFIFOLevelSet(UART0_BASE, UART_FIFO_TX1_8, UART_FIFO_RX1_8);

UARTTxIntModeSet(UART0_BASE, UART_TXINT_MODE_FIFO);

// ROM_UARTIntDisable(UART0_BASE, UART_INT_TX);

ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);

ROM_IntEnable(INT_UART0);

UARTEnable(UART0_BASE);

/**************************ADC configuration***************************************************/

SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); //for ADC0

// SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1); //for ADC1

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);

GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3 | GPIO_PIN_1); //for ADC0


ADCSequenceDisable(ADC0_BASE, 0); //for ADC 0

ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_PROCESSOR, 0);


ADCSequenceStepConfigure(ADC0_BASE, 0,0,ADC_CTL_CH0); //channel 0

ADCSequenceStepConfigure(ADC0_BASE, 0,1,ADC_CTL_CH2 | ADC_CTL_IE | ADC_CTL_END); //for ADC0 //channel 1

ADCSequenceEnable(ADC0_BASE, 0);

ADCIntEnable(ADC0_BASE, 0);

IntEnable(INT_ADC0SS0);

ROM_IntMasterEnable();

/*******written for timer functionalities  *************************************/

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);

ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);

ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, 800);

ROM_IntEnable(INT_TIMER0A);

ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

ROM_TimerEnable(TIMER0_BASE, TIMER_A);

/**************************************************************************************/

while(1)
{

/*******written for timer functionalities on 5/2/15 *************************************/


TimerControlTrigger(TIMER0_BASE,TIMER_A,1);

// TimerControlTrigger(ADC0_BASE, TIMER_BOTH, 2); //*****************check enable either 2 or 1
// TimerLoadSet(ADC0_BASE, TIMER_BOTH, SysCtlClockGet()); //*****load time into display

/*...........................................................................................*/

/***for timer set flag 6/2/2015**********************/

if(set_flag==1)
{

ADCProcessorTrigger(ADC0_BASE, 0);

}

set_flag=0;

count1=0;
//count5=0;

SysCtlDelay(SysCtlClockGet() / 12);

SysCtlDelay(SysCtlClockGet() / 12);

}
}

void
Timer0_Handler(void)
{

int timer_count=0;

TimerIntClear(TIMER0_BASE,0);

while(timer_count!=801)
{
if(timer_count==800)
{
set_flag=1;
}
timer_count++;
}
timer_count=0;

}
/*************************************************************/
void
ADCHandler(void)
{
int voltage_factor,m;

voltage_factor=(float)4095/660;//factor for voltage, scalling voltage is 2.5 for that count is 3102

//current_factor=(float)2481/20; //for 2v the count is 2481.
current_factor=(float)4095/30;

++count1;

ADCIntClear(ADC0_BASE, 0);


//s=ADCSequenceDataGet(ADC0_BASE, 0, pui32ADC0Value); // // Read ADC Value///. modified on 30-12-2014.

//t12=pui32ADC0Value[0]; //here t is the digital count for voltage.

//t13=pui32ADC0Value[1]; //this t1 is the digital count for current.

/*****30-12-2014 modified******************/

pui32ADC0Value[0]=0;

pui32ADC0Value[0] = HWREG(ADC0_BASE + ADC0_O_SSFIFO0);

pui32ADC0Value[1] = HWREG(ADC0_BASE + ADC0_O_SSFIFO0);

/******************************************/
/***********changes on 2/1/15***************/

t=pui32ADC0Value[0];

t1=pui32ADC0Value[1];

/*****************************************/

vlg_value=t/voltage_factor; //here it will gives the total analog voltage ex: 3722/7.44 = 500v

vlg_value1=t/voltage_factor;

current_value=t1/current_factor;

current_value1=t1/current_factor;

}

  • Hi surendra

    You say it's not executed. First, before I even look at your code, I want you to try something.

    While on debug, press play on the code like normal.
    Wait just a few seconds and then press pause (it's pause, not stop). Where is the code? Write it down. Then press play again, wait a bit and then press pause again. Where is the code down?
    Can you return here with that information?
  • Is that written program is correct.
  • I don't understand exactly what you said. Could you reformulate?

    Also, have you read my comment?
  • Luis Afonso said:
    I don't understand exactly

    Nor does the world young tutorial creator - nor does the world...

    While not (rising) to understanding - one suspects poster demands "Full, complete, quick" review of his code - with all imperfections (properly) highlighted/corrected!

    (your rightful/proper/prompting questions - completely dismissed - mais oui?   As forum believes - all posters are skilled, caring, detail driven - no poster "guidance" required!)

    Make (your) full/complete/detailed response - mach schnell as well.  Next...