This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB_stick_update example program NOT powering the USB Thumb Drive

Other Parts Discussed in Thread: EK-TM4C1294XL, TPS2051

MCU: TM4C1294NCPDT

CCS: v6.0.1.0040

-

Hi,

    I loaded the example code provided in the EK-TM4C1294XL folder named USB_stick_update into the MCU. Then loaded an 8 GigaByte capacity USB thumb drive with firmware .bin file FIRMWARE.BIN & inserted the same in the USB Host port of the TM4C1294XL eval kit but upon running the code, the USB thumb drive is NOT getting powered at all (there's a small LED on the USB thumb drive that lights up when the USB drive is powered, it isn't lighting up!!).

    Can anyone tell me what could have been gone wrong? I tried loading the SD to USB copy function of TI-RTOS examples, those are working fine & the USB thumb drive is powered properly & working too!!!

-

Thanks

Regards

Soumyajit