Other Parts Discussed in Thread: ADS1271, HALCOGEN
Hi
I'm doing a school project with this MCU.
I need 12 PWM outputs
24 inputs for encoders, using the N2HET Module
1 SPI for the ADC of the signal.
I was wondering about SPI... Checking the datasheet of the MCU, I saw that there is a SPI4, a MiSPI3 and the MiSPI5 and the MiSPI1. I'm using the ADS1271 and my question is... which pins could I use, that doesnt interfere with the ePWM module or the pins 23, 24, 28, 106, 118, 6, 124, 39, 125, 41, 139, 40, 15, 96, 91, 37, 92, 4, 107, 3, 127, 54 and 9 from N2HET module and one from the ECAP module to be able to have the 24 encoder interruptions and one SPI working for the communication of the ADS?? Because I saw that the MiSPI have many pins but Im not sure if I really need all....
could I only use the MiBSPI3CLK, MiBSPI3NCS[0], MiBSPI3SIMO[0], and the MiBSPI3SOMI[0] and the pin 97 (ECAP) instead of the one from N2HET that is related to the MiSPI3 (pin 96)?
Do I really need the MiBSPI3NENA?
If im using the ADS1271 which pins do i rally need for SPI??
best regards