This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Micro controller to Ethernet.

How can i transmit the data from  one micro controller to other micro controller with help of Ethernet.

  • Hello Surendra,

    What type of n/w topology are you using. If it is a P2P then why go through ethernet. You can have simpler interfaces like UART, SPI or I2C.

    Regards
    Amit
  • surendra malampati said:
    transmit the data ... between 2 MCUs...with help of Ethernet.

    Ethernet - described here as a, "Help?"   Really?

    Any of the MCU's (other) serial interfaces stand ready to far quicker - and easier, "Help!"

    New cars have many, many MCUs - and almost all are interconnected - yet few employ Ethernet.   (might there be a reason CAN is far more popular?)