can HET be used for timer output and GIO output at the same time? please explain.
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
can HET be used for timer output and GIO output at the same time? please explain.
thanks.
Hi Pavithra,
Yes, you can use some HET pins as GPIO and others as functional HET pins(PWM or capture). You don't need to specially configure anything for this. As long as you're not using a particular pin for HET functionality, you can use it for GPIO. For more info, you can check the TRM (N2HET Module > N2HET Functional Description > I/O Control).
I don't understand the second question completely. If you want a physical pin (lets say pin A13) to be tied to GPIO functionality, you can mux the output buffer to N2HET1[17] (instead of EMIF_nOE) and use the A13 pin as GPIO.
Thanks and Regards,
Vineeth