Hello.
Hardware: TI Tiva C Series TM4C123GXL Launchpad, TI LM1086IT-5.0/NOPB LDO Voltage Regulator and a 9V battery (a little used).
Software: Basic 'Blink' example from Energia
Problem: The programme does not run when the board gets its power (to VBUS) from the 9V battery, via the 5V regulator (my multimeter reads 4.9V). The LED does not blink at all while the board is powered by the battery. However, the green power LED is on. I did check and the LED blinks when the board is powered by my PC via USB.
Can anyone help, please?
Thank you.
Alex