This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UDP Using Static IP not working,in TM4C1294NCPDT

Other Parts Discussed in Thread: EK-TM4C1294XL

Hello,

I am trying to send UDP FROM CONTROLLER TO PC ,ITS NOT WORKING,I TRIED IN ENET IO AND SUCCEDED,any recommendations please

//*****************************************************************************
//
// enet_lwip.c - Sample WebServer Application using lwIP.
//
// Copyright (c) 2013-2014 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************

#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include <stdlib.h>
#include <stdio.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/flash.h"
#include "driverlib/interrupt.h"
#include "driverlib/gpio.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "utils/locator.h"
#include "utils/lwiplib.h"
#include "utils/ustdlib.h"
#include "utils/uartstdio.h"
#include "httpserver_raw/httpd.h"
#include "drivers/pinout.h"
#include "lwip/inet.h"


//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Ethernet with lwIP (enet_lwip)</h1>
//!
//! This example application demonstrates the operation of the Tiva
//! Ethernet controller using the lwIP TCP/IP Stack. DHCP is used to obtain
//! an Ethernet address. If DHCP times out without obtaining an address,
//! AutoIP will be used to obtain a link-local address. The address that is
//! selected will be shown on the UART.
//!
//! UART0, connected to the ICDI virtual COM port and running at 115,200,
//! 8-N-1, is used to display messages from this application. Use the
//! following command to re-build the any file system files that change.
//!
//! ../../../../tools/bin/makefsfile -i fs -o enet_fsdata.h -r -h -q
//!
//! For additional details on lwIP, refer to the lwIP web page at:
//! savannah.nongnu.org/.../lwip
//
//*****************************************************************************

//*****************************************************************************
//
// Defines for setting up the system clock.
//
//*****************************************************************************
#define SYSTICKHZ 100
#define SYSTICKMS (1000 / SYSTICKHZ)

//*****************************************************************************
//
// Interrupt priority definitions. The top 3 bits of these values are
// significant with lower values indicating higher priority interrupts.
//
//*****************************************************************************
#define SYSTICK_INT_PRIORITY 0x80
#define ETHERNET_INT_PRIORITY 0xC0
extern void udp_init(void);
//*****************************************************************************
//
// The current IP address.
//
//*****************************************************************************
uint32_t g_ui32IPAddress;

//*****************************************************************************
//
// The system clock frequency.
//
//*****************************************************************************
uint32_t g_ui32SysClock;


uint32_t sourceaddr, netmask,gateway;
struct ip_addr udpDestIpAddr;
struct udp_pcb *my_pcb;
struct pbuf* pbuf1;
char buf [120];


//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// Display an lwIP type IP Address.
//
//*****************************************************************************
void
DisplayIPAddress(uint32_t ui32Addr)
{
char pcBuf[16];

//
// Convert the IP Address into a string.
//
usprintf(pcBuf, "%d.%d.%d.%d", ui32Addr & 0xff, (ui32Addr >> 8) & 0xff,
(ui32Addr >> 16) & 0xff, (ui32Addr >> 24) & 0xff);

//
// Display the string.
//
UARTprintf(pcBuf);
}

//*****************************************************************************
//
// Required by lwIP library to support any host-related timer functions.
//
//*****************************************************************************
void
lwIPHostTimerHandler(void)
{
uint32_t ui32Idx, ui32NewIPAddress;

//
// Get the current IP address.
//
ui32NewIPAddress = lwIPLocalIPAddrGet();

//
// See if the IP address has changed.
//
if(ui32NewIPAddress != g_ui32IPAddress)
{
//
// See if there is an IP address assigned.
//
if(ui32NewIPAddress == 0xffffffff)
{
//
// Indicate that there is no link.
//
UARTprintf("Waiting for link.\n");
}
else if(ui32NewIPAddress == 0)
{
//
// There is no IP address, so indicate that the DHCP process is
// running.
//
UARTprintf("Waiting for IP address.\n");
}
else
{
//
// Display the new IP address.
//
UARTprintf("IP Address: ");
DisplayIPAddress(ui32NewIPAddress);
UARTprintf("\nOpen a browser and enter the IP address.\n");
}

//
// Save the new IP address.
//
g_ui32IPAddress = ui32NewIPAddress;

//
// Turn GPIO off.
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, ~GPIO_PIN_1);
}

//
// If there is not an IP address.
//
if((ui32NewIPAddress == 0) || (ui32NewIPAddress == 0xffffffff))
{
//
// Loop through the LED animation.
//

for(ui32Idx = 1; ui32Idx < 17; ui32Idx++)
{

//
// Toggle the GPIO
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1,
(MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1) ^
GPIO_PIN_1));

SysCtlDelay(g_ui32SysClock/(ui32Idx << 1));
}
}
}

//*****************************************************************************
//
// The interrupt handler for the SysTick interrupt.
//
//*****************************************************************************
void
SysTickIntHandler(void)
{
//
// Call the lwIP timer handler.
//
lwIPTimer(SYSTICKMS);
}

//*****************************************************************************
//
// This example demonstrates the use of the Ethernet Controller.
//
//*****************************************************************************
int
main(void)
{
uint32_t ui32User0, ui32User1;
uint8_t pui8MACArray[8];

//
// Make sure the main oscillator is enabled because this is required by
// the PHY. The system must have a 25MHz crystal attached to the OSC
// pins. The SYSCTL_MOSC_HIGHFREQ parameter is used when the crystal
// frequency is 10MHz or higher.
//
SysCtlMOSCConfigSet(SYSCTL_MOSC_HIGHFREQ);

//
// Run from the PLL at 120 MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);

//
// Configure the device pins.
//
PinoutSet(true, false);

//
// Configure UART.
//
UARTStdioConfig(0, 115200, g_ui32SysClock);
// Enable all GPIO banks.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);

//
// Clear the terminal and print banner.
//
UARTprintf("\033[2J\033[H");
UARTprintf("Ethernet lwIP example\n\n");

//
// Configure Port N1 for as an output for the animation LED.
//
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_1);

//
// Initialize LED to OFF (0)
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, ~GPIO_PIN_1);

//
// Configure SysTick for a periodic interrupt.
//
MAP_SysTickPeriodSet(g_ui32SysClock / SYSTICKHZ);
MAP_SysTickEnable();
MAP_SysTickIntEnable();

//
// Configure the hardware MAC address for Ethernet Controller filtering of
// incoming packets. The MAC address will be stored in the non-volatile
// USER0 and USER1 registers.
//
MAP_FlashUserGet(&ui32User0, &ui32User1);
if((ui32User0 == 0xffffffff) || (ui32User1 == 0xffffffff))
{
//
// We should never get here. This is an error if the MAC address has
// not been programmed into the device. Exit the program.
// Let the user know there is no MAC address
//
UARTprintf("No MAC programmed!\n");
while(1)
{
}
}

//
// Tell the user what we are doing just now.
//
UARTprintf("Waiting for IP.\n");

//
// Convert the 24/24 split MAC address from NV ram into a 32/16 split MAC
// address needed to program the hardware registers, then program the MAC
// address into the Ethernet Controller registers.
//
pui8MACArray[0] = ((ui32User0 >> 0) & 0xff);
pui8MACArray[1] = ((ui32User0 >> 8) & 0xff);
pui8MACArray[2] = ((ui32User0 >> 16) & 0xff);
pui8MACArray[3] = ((ui32User1 >> 0) & 0xff);
pui8MACArray[4] = ((ui32User1 >> 8) & 0xff);
pui8MACArray[5] = ((ui32User1 >> 16) & 0xff);

//
// Initialize the lwIP library, using static ip.
//

sourceaddr=inet_addr("28.1.17.172");
netmask=inet_addr("0.0.255.255");
gateway=inet_addr("3.0.17.172");

lwIPInit(g_ui32SysClock,pui8MACArray,sourceaddr,netmask,gateway,IPADDR_USE_STATIC);
//
// Setup the device locator service.
//
LocatorInit();
LocatorMACAddrSet(pui8MACArray);
LocatorAppTitleSet("EK-TM4C1294XL enet_io");

//
// Initialize a sample httpd server.
//
udp_init();

struct udp_pcb * mypcb;
mypcb = udp_new();
if (mypcb == NULL)
{
UARTprintf("udp failed.\n");
}
else
{
UARTprintf("udp up.\n");
}

if (udp_bind(mypcb, IP_ADDR_ANY, 8760) != ERR_OK)
{
UARTprintf("udp bind failed.\n");
}
//
// Set the interrupt priorities. We set the SysTick interrupt to a higher
// priority than the Ethernet interrupt to ensure that the file system
// tick is processed if SysTick occurs while the Ethernet handler is being
// processed. This is very likely since all the TCP/IP and HTTP work is
// done in the context of the Ethernet interrupt.
//
MAP_IntPrioritySet(INT_EMAC0, ETHERNET_INT_PRIORITY);
MAP_IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY);

//
// Loop forever. All the work is done in interrupt handlers.
//
while(1)
{
static int n = 0;
pbuf1 = pbuf_alloc(PBUF_TRANSPORT, 100, PBUF_RAM);
pbuf1->payload = (void*)buf;
pbuf1->tot_len = 22; //data length
pbuf1->len = 20;

buf[0] = 'A';
buf[1] = 'A';
usprintf(&buf[4], " abcABC1230000000000 %d", n++);
IP4_ADDR(&udpDestIpAddr,172,17,2,30);
udp_sendto(mypcb, pbuf1,&udpDestIpAddr,1001);
pbuf_free(pbuf1);
}
}

Regards,

Krishnan