Other Parts Discussed in Thread: TM4C1294NCPDT
Hello,
I am trying to get data from FPGA .I was able to read data.Now my requirement is FPGA will give interrupt and then i have to read data i made a sample code choose GPIO_PK4_EPI0S32 as interrupt pin.I am attaching my code ,plese help me in diasbling interrupt and reading data from FPGA
#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include <stdlib.h>
#include <stdio.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_nvic.h"
#include "inc/hw_types.h"
#include "inc/hw_epi.h"
#include "inc/hw_gpio.h"
#include <driverlib/gpio.h>
#include "driverlib/epi.h"
#include "driverlib/flash.h"
#include "driverlib/interrupt.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/timer.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/pin_map.h"
#include "utils/locator.h"
#include "utils/lwiplib.h"
#include "utils/uartstdio.h"
#include "driverlib/uart.h"
#include "utils/ustdlib.h"
#include "drivers/pinout.h"
//#include "inc/tm4c1294ncpdt.h"
#include "io.h"
#include "cgifuncs.h"
#include "lwip/inet.h"
//*****************************************************************************
//
// Defines for setting up the system clock.
//
//*****************************************************************************
#define SYSTICKHZ 100
#define SYSTICKMS (1000 / SYSTICKHZ)
//*****************************************************************************
//
// Interrupt priority definitions. The top 3 bits of these values are
// significant with lower values indicating higher priority interrupts.
//
//*****************************************************************************
#define SYSTICK_INT_PRIORITY 0x80
#define ETHERNET_INT_PRIORITY 0xC0
////////////////////////////////////////////////////////////////////////////////////////
uint32_t sourceaddr, netmask,gateway;
struct ip_addr udpDestIpAddr;
//*****************************************************************************
#define FLAG_TICK 0
static volatile unsigned long g_ulFlags;
//*****************************************************************************
//
// External Application references.
//
//*****************************************************************************
extern void udp_init(void);
//*****************************************************************************
//
// SSI tag indices for each entry in the g_pcSSITags array.
//
//*****************************************************************************
#define SSI_INDEX_LEDSTATE 0
#define SSI_INDEX_FORMVARS 1
#define SSI_INDEX_SPEED 2
//*****************************************************************************
#define NUM_CONFIG_SSI_TAGS (sizeof(g_pcConfigSSITags) / sizeof (char *))
//*****************************************************************************
// CGI URI indices for each entry in the g_psConfigCGIURIs array.
//
//*****************************************************************************
#define CGI_INDEX_CONTROL 0
#define CGI_INDEX_TEXT 1
//*****************************************************************************
//
// The number of individual CGI URIs that are configured for this system.
//
//*****************************************************************************
#define NUM_CONFIG_CGI_URIS (sizeof(g_psConfigCGIURIs) / sizeof(tCGI))
//*****************************************************************************
//
// The file sent back to the browser by default following completion of any
// of our CGI handlers. Each individual handler returns the URI of the page
// to load in response to it being called.
//
//*****************************************************************************
#define DEFAULT_CGI_RESPONSE "/io_cgi.ssi"
// The current IP address.
//
//*****************************************************************************
uint32_t g_ui32IPAddress;
//*****************************************************************************
//
// The system clock frequency. Used by the SD card driver.
//
//*****************************************************************************
uint32_t g_ui32SysClock;
uint32_t g_ui32IntMode;
///////////////////////////////////////////////////
struct udp_pcb *my_pcb;
struct pbuf* pbuf1;
char buf [120];
char *g_pusEPIFPGA;
unsigned long index;
char *datasram;
int i=0;
unsigned short *cptr;
unsigned char cval;
volatile uint32_t g_ui32GPIOA;
////////////**************sdram
//char *cptr = (char *)0x20000500;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
////////////**********************************8///////////////////////////
/*void GPIOPinTypeEPI(uint32_t ui32Port,uint8_t ui8Pins)
{
// Check the arguments.
ASSERT(GPIOBaseValid(ui32Port));
// Make the pin(s) be peripheral controlled.
GPIODirModeSet(ui32Port, ui8Pins, GPIO_DIR_MODE_HW);
// Set the pad(s) for standard push-pull operation.
GPIOPadConfigSet(ui32Port, ui8Pins, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
}
*/
//*****************************************************************************
//
// The interrupt handler for the SysTick interrupt.
//
//*****************************************************************************
void
SysTickIntHandler(void)
{
//
// Call the lwIP timer handler.
//
lwIPTimer(SYSTICKMS);
}
///////////////////////////////////////////////////////////////////
void GPIOAIntHandler(void)
{
// Clear the GPIO interrupt.
GPIOIntClear(GPIO_PORTA_BASE, GPIO_PK4_EPI0S32);
}
void EPI_Init(void)
{
// Enable EPI0.
SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);
//Configure EPIO
EPIDividerSet(EPI0_BASE, 1);
EPIModeSet(EPI0_BASE, EPI_MODE_HB16);
EPIConfigHB16Set(EPI0_BASE,(EPI_HB16_MODE_SRAM | EPI_HB16_WRWAIT_1 |EPI_HB16_RDWAIT_1 | EPI_HB16_WORD_ACCESS), 0);
EPIAddressMapSet(EPI0_BASE, EPI_ADDR_PER_BASE_C | EPI_ADDR_PER_SIZE_256B);////0xC0000000
//EPIFIFOConfig(EPI0_BASE, EPI_FIFO_CONFIG_TX_EMPTY | EPI_FIFO_CONFIG_RX_1_4);
// Configure GPIO
GPIOPinConfigure(GPIO_PB3_EPI0S28); //RD
GPIOPinConfigure(GPIO_PP2_EPI0S29); //WR
GPIOPinConfigure(GPIO_PK0_EPI0S0); //D0
GPIOPinConfigure(GPIO_PK1_EPI0S1); //D1
GPIOPinConfigure(GPIO_PK2_EPI0S2); //D2
GPIOPinConfigure(GPIO_PK3_EPI0S3); //D3
GPIOPinConfigure(GPIO_PC7_EPI0S4); //D4
GPIOPinConfigure(GPIO_PC6_EPI0S5); //D5
GPIOPinConfigure(GPIO_PC5_EPI0S6); //D6
GPIOPinConfigure(GPIO_PC4_EPI0S7); //D7
GPIOPinConfigure(GPIO_PA6_EPI0S8); //D8
GPIOPinConfigure(GPIO_PA7_EPI0S9); //D9
GPIOPinConfigure(GPIO_PG1_EPI0S10); //D10
GPIOPinConfigure(GPIO_PG0_EPI0S11); //D11
GPIOPinConfigure(GPIO_PM3_EPI0S12); //D12
GPIOPinConfigure(GPIO_PM2_EPI0S13); //D13
GPIOPinConfigure(GPIO_PM1_EPI0S14); //D14
GPIOPinConfigure(GPIO_PM0_EPI0S15); //D15
GPIOPinConfigure(GPIO_PL0_EPI0S16); //A0
GPIOPinConfigure(GPIO_PL1_EPI0S17); //A1
GPIOPinConfigure(GPIO_PL2_EPI0S18); //A2
GPIOPinConfigure(GPIO_PL3_EPI0S19); //A3
GPIOPinConfigure(GPIO_PQ0_EPI0S20); //A4
GPIOPinConfigure(GPIO_PQ1_EPI0S21); //A5
GPIOPinConfigure(GPIO_PQ2_EPI0S22); //A6
GPIOPinConfigure(GPIO_PQ3_EPI0S23); //A7
GPIOPinConfigure(GPIO_PK7_EPI0S24); //A8
GPIOPinConfigure(GPIO_PK6_EPI0S25); //A9
GPIOPinConfigure(GPIO_PL4_EPI0S26); //A10
GPIOPinConfigure(GPIO_PB2_EPI0S27); //A11
GPIOPinConfigure(GPIO_PP3_EPI0S30); //CHIP SELECT
GPIOPinConfigure(GPIO_PK5_EPI0S31); //CLK
GPIOPinConfigure(GPIO_PK4_EPI0S32); //IRDY
GPIOPinConfigure(GPIO_PN5_EPI0S35); //CRE
GPIOPinTypeEPI(GPIO_PORTA_BASE, 0xC0);
GPIOPinTypeEPI(GPIO_PORTB_BASE, 0x0C);
GPIOPinTypeEPI(GPIO_PORTC_BASE, 0xF0);
GPIOPinTypeEPI(GPIO_PORTG_BASE, 0x03);
GPIOPinTypeEPI(GPIO_PORTK_BASE, 0xFF);
GPIOPinTypeEPI(GPIO_PORTL_BASE, 0x1F);
GPIOPinTypeEPI(GPIO_PORTM_BASE, 0x0F);
GPIOPinTypeEPI(GPIO_PORTN_BASE, 0x20);
GPIOPinTypeEPI(GPIO_PORTP_BASE, 0x0C);
GPIOPinTypeEPI(GPIO_PORTQ_BASE, 0x0F);
GPIOPadConfigSet (GPIO_PORTA_BASE, 0xC0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTB_BASE, 0x0C, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTC_BASE, 0xF0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTG_BASE, 0x03, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTK_BASE, 0xFF, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTL_BASE, 0x1F, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTM_BASE, 0x0F, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTN_BASE, 0x20, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTP_BASE, 0x0C, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet (GPIO_PORTQ_BASE, 0x0F, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet (GPIO_PORTA_BASE, 0xC0, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTB_BASE, 0x0C, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTC_BASE, 0xF0, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTG_BASE, 0x03, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTK_BASE, 0xFF, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTL_BASE, 0x1F, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTM_BASE, 0x0F, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTN_BASE, 0x20, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTP_BASE, 0x0C, GPIO_DIR_MODE_HW);
GPIODirModeSet (GPIO_PORTQ_BASE, 0x0F, GPIO_DIR_MODE_HW);
}
void fpga_read()
{
#if 0
char *temp;
datasram = ( char *)malloc(1456*sizeof( char));
temp = datasram;
g_pusEPIFPGA = (char*)0xC0000000;
for(i = 0;i<144;i++)
{
*datasram = g_pusEPIFPGA[index];
*datasram++;
}
datasram = temp;
free(datasram);
#endif
unsigned short *cptr;// = (unsigned char *)0xC0000000;
//cval = *cptr;
cptr = (unsigned short *)0xC0000000;
while(i<=127)
{
cval = *cptr;
printf("Address of var1 variable: %x\n", *cptr );
cptr = cptr++;
i++;
}
cptr = (unsigned short *)0xC0000024;
cval = *cptr;
cptr = (unsigned short *)0xC0000004;
cval = *cptr;
cptr++;
cptr = (unsigned short *)0xC0000005;
cval = *cptr;
cptr++;
cptr = (unsigned short *)0xC0000256;
cval = *cptr;
cptr++;
}
//*****************************************************************************
//
// The interrupt handler for the timer used to pace the animation.
//
//*****************************************************************************
void
AnimTimerIntHandler(void)
{
//
// Clear the timer interrupt.
//
MAP_TimerIntClear(TIMER2_BASE, TIMER_TIMA_TIMEOUT);
//
// Indicate that a timer interrupt has occurred.
//
HWREGBITW(&g_ulFlags, FLAG_TICK) = 1;
}
//*****************************************************************************
//
// Display an lwIP type IP Address.
//
//*****************************************************************************
void
DisplayIPAddress(uint32_t ui32Addr)
{
char pcBuf[16];
//
// Convert the IP Address into a string.
//
usprintf(pcBuf, "%d.%d.%d.%d", ui32Addr & 0xff, (ui32Addr >> 8) & 0xff,
(ui32Addr >> 16) & 0xff, (ui32Addr >> 24) & 0xff);
//
// Display the string.
//
UARTprintf(pcBuf);
}
//*****************************************************************************
//
// Required by lwIP library to support any host-related timer functions.
//
//*****************************************************************************
void
lwIPHostTimerHandler(void)
{
uint32_t ui32Idx, ui32NewIPAddress;
//
// Get the current IP address.
//
ui32NewIPAddress = lwIPLocalIPAddrGet();
//
// See if the IP address has changed.
//
if(ui32NewIPAddress != g_ui32IPAddress)
{
//
// See if there is an IP address assigned.
//
if(ui32NewIPAddress == 0xffffffff)
{
//
// Indicate that there is no link.
//
UARTprintf("Waiting for link.\n");
}
else if(ui32NewIPAddress == 0)
{
//
// There is no IP address, so indicate that the DHCP process is
// running.
//
UARTprintf("Waiting for IP address.\n");
}
else
{
//
// Display the new IP address.
//
UARTprintf("IP Address: ");
DisplayIPAddress(ui32NewIPAddress);
}
//
// Save the new IP address.
//
g_ui32IPAddress = ui32NewIPAddress;
}
//
// If there is not an IP address.
//
if((ui32NewIPAddress == 0) || (ui32NewIPAddress == 0xffffffff))
{
//
// Loop through the LED animation.
//
for(ui32Idx = 1; ui32Idx < 100; ui32Idx++) //was < 17
{
//
// Toggle the GPIO
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1,
(MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1) ^
GPIO_PIN_1));
SysCtlDelay(g_ui32SysClock/(ui32Idx << 1));
}
}
}
//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = ROM_UARTIntStatus(UART0_BASE, true);
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART0_BASE, ui32Status);
//
// Loop while there are characters in the receive FIFO.
//
while(ROM_UARTCharsAvail(UART0_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
ROM_UARTCharPutNonBlocking(UART0_BASE,
ROM_UARTCharGetNonBlocking(UART0_BASE));
}
}
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
ROM_UARTCharPutNonBlocking(UART0_BASE, *pui8Buffer++);
}
}
//*****************************************************************************
int main(void)
{
uint8_t pui8MACArray[8];
// Make sure the main oscillator is enabled because this is required by
// the PHY. The system must have a 25MHz crystal attached to the OSC
// pins. The SYSCTL_MOSC_HIGHFREQ parameter is used when the crystal
// frequency is 10MHz or higher.
//
SysCtlMOSCConfigSet(SYSCTL_MOSC_HIGHFREQ);
//
// Run from the PLL at 120 MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
UARTStdioConfig(0, 115200, g_ui32SysClock);
/////Enable all GPIO BANKS////////////////////////////
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
// SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
//
// Configure the device pins.
//
PinoutSet(true, false);
//
// Configure debug port for internal use.
//
UARTStdioConfig(0, 115200, g_ui32SysClock);
//
// Clear the terminal and print a banner.
//
UARTprintf("\033[2J\033[H");
UARTprintf("Ethernet IO Example\n\n");
//
// Configure SysTick for a periodic interrupt.
//
MAP_SysTickPeriodSet(g_ui32SysClock / SYSTICKHZ);
MAP_SysTickEnable();
MAP_SysTickIntEnable();
GPIOPinConfigure(GPIO_PK4_EPI0S32);//irdy
GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, GPIO_PK4_EPI0S32);
GPIOPadConfigSet(GPIO_PORTA_BASE, GPIO_PK4_EPI0S32, GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD);
GPIOIntTypeSet(GPIO_PORTA_BASE, GPIO_PK4_EPI0S32, GPIO_FALLING_EDGE );
GPIOIntEnable(GPIO_PORTA_BASE, GPIO_PK4_EPI0S32);
IntEnable(INT_GPIOA);
// Enable interrupts to the processor.
//
ROM_IntMasterEnable();
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable interrupts to the processor.
//
EPI_Init();
fpga_read();
//
// Convert the 24/24 split MAC address from NV ram into a 32/16 split
// MAC address needed to program the hardware registers, then program
// the MAC address into the Ethernet Controller registers.
//
pui8MACArray[0] = 0x01;
pui8MACArray[1] = 0x02;
pui8MACArray[2] = 0x03;
pui8MACArray[3] = 0x01;
pui8MACArray[4] = 0x02;
pui8MACArray[5] = 0x03;
//
// Initialze the lwIP library, using DHCP.
sourceaddr=inet_addr("28.1.17.172");
netmask=inet_addr("0.0.255.255");
gateway=inet_addr("3.0.17.172");
lwIPInit(g_ui32SysClock,pui8MACArray,sourceaddr,netmask,gateway,IPADDR_USE_STATIC);
LocatorInit();
LocatorMACAddrSet(pui8MACArray);
// ***************************uart//////////////
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Configure the UART for 115,200, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART0_BASE, g_ui32SysClock, 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
//
// Enable the UART interrupt.
//
ROM_IntEnable(INT_UART0);
ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
//
// Prompt for text to be entered.
//
UARTSend((uint8_t *)"hiiii hw r u tfrg ", 16);
UARTprintf("udp failed.\n");
/////////////*********************************
udp_init();
struct udp_pcb * mypcb;
mypcb = udp_new();
if (mypcb == NULL)
{
UARTprintf("udp failed.\n");
}
else
{
UARTprintf("udp up.\n");
}
if (udp_bind(mypcb, IP_ADDR_ANY, 8760) != ERR_OK)
{
UARTprintf("udp bind failed.\n");
}
//
// Set the interrupt priorities. We set the SysTick interrupt to a higher
// priority than the Ethernet interrupt to ensure that the file system
// tick is processed if SysTick occurs while the Ethernet handler is being
// processed. This is very likely since all the TCP/IP and HTTP work is
// done in the context of the Ethernet interrupt.
//
MAP_IntPrioritySet(INT_EMAC0, ETHERNET_INT_PRIORITY);
MAP_IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY);
// Initialize IO controls
//
io_init();
//
// Loop forever, processing the on-screen animation. All other work is
// done in the interrupt handlers.
//
while(1)
{
//
// Wait for a new tick to occur.
//
while(!g_ulFlags)
{
//
// Do nothing.
//
}
//
//
// Clear the flag now that we have seen it.
//
HWREGBITW(&g_ulFlags, FLAG_TICK) = 0;
//
// Toggle the GPIO
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1,
(MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1) ^
GPIO_PIN_1));
//
// Transmit to UDP
//
//static int n = 0;
pbuf1 = pbuf_alloc(PBUF_TRANSPORT, 100, PBUF_RAM);
pbuf1->payload = cptr; //(void*)buf;
pbuf1->tot_len = 22; //data length
pbuf1->len = 20;
// *cptr = 'A'; cptr++;
//*cptr = 'A'; cptr++;
// *cptr = 'A'; cptr++;
// *cptr = 'A'; cptr++;
//*cptr = 'A'; cptr++;
// buf[0] = 'A';
//buf[1] = 'A';
//usprintf(&buf[4], " abcABC1230000000000 %d", n++);
IP4_ADDR(&udpDestIpAddr,172,17,2,30);
udp_sendto(mypcb, pbuf1,&udpDestIpAddr,1001);
pbuf_free(pbuf1);
}
}
Regards,
Krishnan