Other Parts Discussed in Thread: TM4C129XNCZAD
Hi there,
I am looking to install a 7 inch, 800x480 LCD panel on the DK-TM4C129X Tiva display. My LCD has a 40-pin connector, the Tiva board accepts a 60 pin one. The pin-out of my LCD panel is the exact same as the Newhaven LCD found on the TI Sitara boards. My question is: would it be feasible to make a physical adapter from 60-pin to 40-pin and then take a Sitara LCD driver and adapt it to the Tiva board? How easy would it be to adapt the code? If not, are there any LCD's that would fit the Tiva 60-pin connector?
Here is the Tiva Kentec LCD pin-out (page 6):
http://www.kentec.com.hk/images/UploadFile/20111115190922-7.pdf
Here is the Sitara Newhaven LCD pin-out (page 4):
http://www.newhavendisplay.com/specs/NHD-4.3-480272EF-ATXL-T.pdf
Thank you in advance!