Other Parts Discussed in Thread: EK-TM4C1294XL, LMFLASHPROGRAMMER
Hi,
My aim is to upgrade the firmware for EK-TM4C1294XL board while its running.
I want to to extent enet_io example. My plan is to create a webpage in which to provide a link to select the .bin file from local machine and than use this .bin file for upgrade. But I am not able to figure out from where to start. Board will be currently only on local area network.
I seen in one of the post http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/p/376880/1337869 but I am not able to add the function of ConfigureEnet() and UpdateBOOTP() on my code.
Can anybody help how to achieve this ?
I am using CCSv6 on 64-bit windows 8.
Thanks,
Bhavesh