Other Parts Discussed in Thread: TM4C123BH6PGE, TM4C123GH6PGE
Hi,
I am using 22 analog inputs on a TM4C123BH6PGE. My prototype board works perfectly. My production board, running the same code, has a problem.
The prototype board has chip marked....
980 YF TM4C123B H6PGEI 35AVELW G4
The production board has chip marked....
980 YF TM4C123B H6PGEI 35AVENW G4
I can't find out how to read the silicon revision on the chip.
I am using PE3 for AIN0, this is driven directly by an opamp which is buffering a pot. It appears that the voltage presented to this pin affects all the other adc channels as if the input multiplexer is not working properly. This happens even if I do not sample this channel. Cutting the track to this pin stops the problem happening, so it seems it is not a board error.
I can't find a reference to this in any of the errata, but may be I missed something?
Can anybody help please?
Thanks, Richard
I put these two lines at the top of each file. Is this right?...
#define PART_TM4C123GH6PGE
#define TARGET_IS_BLIZZARD_RA1
My ADC initialisation code is....
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_7); //ch20
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_6); //ch21
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_5); //ch8
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_4); //ch9
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3); //ch0
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2); //ch1
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1); //ch2
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0); //ch3
ROM_ADCSequenceDisable(ADC0_BASE, 1); //disable sequence before we change it
ROM_ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0); //select processor (software) trigger
ROM_ADCSequenceStepConfigure(ADC0_BASE, 3, 0, 0 | ADC_CTL_IE | ADC_CTL_END);
ROM_ADCIntClear(ADC0_BASE, 3); //clear the interrupt status flag
ROM_ADCSequenceEnable(ADC0_BASE, 3); //enable sequence
My ADC sampling function is....
unsigned long getADC0(unsigned long channel) //channel is bit mask eg ADC_CTL_CH0
{
uint32_t ADC0_value[1];
//ROM_ADCSequenceDisable(ADC0_BASE, 3); //disable sequence 3 before we change it; doesn't seem to be necessary
ROM_ADCSequenceStepConfigure(ADC0_BASE, 3, 0, channel | ADC_CTL_IE | ADC_CTL_END);
//ROM_ADCSequenceEnable(ADC0_BASE, 3); //enable
ROM_ADCProcessorTrigger(ADC0_BASE, 3); //trigger
while(!ROM_ADCIntStatus(ADC0_BASE, 3, false)) //wait complete
{
}
ROM_ADCIntClear(ADC0_BASE, 3); //clear the ADC interrupt flag
ROM_ADCSequenceDataGet(ADC0_BASE, 3, ADC0_value); //read ADC Value
return ADC0_value[0];
}