This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100v2-arm Emulator incompatible with DK-TM4C129X Dev Board

I have a DK-TM4C129X Development Board.  I also have an XDS100 emulator (p/n TMDSEMU100V20-ARM).  The connectors do not match.

The dev board has a 20-pin emulator connector at location J1; the pitch seems to be 0.05". 

The emulator has a 10-pin 0.05" connector and a 20-pin 0.1" connector.  The supplied cables are 10-pin to 10-pin 0.05pitch and 20-pin to 20-pin 0.1 pitch. 

Is there an adapter available to transform between the two sizes of 20-pin connectors?