This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSLib request



Hi,

I just got the new version (2.2) of the TPSLib.  It's a huge step from a documentation standpoint from the previous version, thank you!

 

I would like to request some more work to be done though.  When the library is built there are currently 8 warnings generated and 100 TODOs.  It would be great to see both of these numbers get to 0.  I realize software resources at any company are  limited, so taking time to get rid of these may not get a high priority, but if someone if building the library like I am (because I have to slightly modify it because of false errors generated by the TPS chip), they are a huge inconvenience.  People start ignoring warnings altogether, and don't take care of warnings they should.  It also makes it difficult to use the TODO keyword in out own code because of the large number that is in the TPS lib.  If the documentation isn't going to be completed that's fine, but please at least remove the todo keyword.

 

Thanks,

David