This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Disable network functions from PK4 pin

Hi all,

I have a project on the TM4C1294XL board, based on the TCP echo example with ti rtos (2_10_01_38).

I want to use the PK4 port as a normal GPIO output pin. Unfortunately I always get a signal (each ms) from the Ethernet driver when a connection is established, which is an overlay to my controls of the pin.

A workaround might be the usage as a "dead" PWM pin (where no overlays occur) with inverted output, but I would rather go with a clean solution, if possible.

I managed to switch of PF0 and PF4 as the Ethernet- LEDs, but i have no idea where to deactivate any further functionality on PK4.

Any ideas for me where to look?


Thank you!

Best regards, Simon