Hai,
I interfaced a character LCD display with TIVA C launchpad and it was successfully worked but now its fails with same code and connection on another launchpad i set all the pins of port B as out put ,and write 0xff, but PB6 and PB7 have only up to 2.2 volts as output voltage. on other hand its 3.3 volts in another launchpad...i think it may be the reason for the improper working of the LCD.please let me know hows this happened? how its possible to set back to 3.3 volts as output...is it any manufacturing defect or programmatic error?