Recently I integrated ROM_FlashErase and ROM_FlashProgram into our application. Once we integrated them, we started missing a small number of interrupts (0.13%).
I might be missing it, but I don't see anything in the TivaWare manual or the TM4C datasheet that says accessing flash might cause interrupts to be missed or increase their latency. I now have the problem fixed (0.00% interrupt loss), but I had to move FlashErase, FlashProgram, and our interrupts into RAM.
Can someone at TI please confirm this is in required and if anything else is required.
Many thanks,
JR