This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Availability of TM4C1294 device



Hello,

   We have been developing some IoT based devices on your TM4C1294 platform. But we are worried to hear that in Kolkata (india) these devices are limited for supply. Specifically element14 said that they can arrange these Cortex M MCUs from TI only after 3 weeks. Im worried as I have worked a lot to kind of insisted the board to work on TM4C1294 platform when they wanted to go for others (like ENC28J with some other MCU). Is large scale availability through channels an issue still now , or this is a temporary phase or this MCU is being phased out sometime soon (seems impossible though).

Im really worried, please suggest

  • Hello Turjasu

    Digikey has the devices in lot and ready to ship. Normally it takes a week from Digikey

    Regards
    Amit
  • TURJASU PYNE1 said:
     We have been developing some IoT based devices on your TM4C1294 platform. But we are worried to hear that in Kolkata (india) these devices are limited for supply. Specifically element14 said that they can arrange these Cortex M MCUs from TI only after 3 weeks.

     On current market this is a very short time and sound like "on stock"!!!

    TURJASU PYNE1 said:
    TM4C1294 platform when they wanted to go for others (like ENC28J with some other MCU)

     If your target is a very slow 10Mbit network with so prehistoric device ...

    TURJASU PYNE1 said:
    Im really worried, please suggest

    then no need for DMA driven full 100Mbps network.. your platform is that other..

    NOne really involved on production can write a so kid_diy driven text!!! Sorry that is not your chip, your way is hobby maket DIL and old devices, production plant and market time are different things, your word exposed no knowledge of industrial eyesight.