Other Parts Discussed in Thread: EK-TM4C123GXL
Hello everyone,
I plan to use ARM MCU in my next application/project and I picked EK-TM4C123GXL board as a starting point. So far I've downloaded all document and software packages that are needed to work with and was able to get lab2 in the workshop package up and running. However, I've noticed something very unusual with my Launchpad board compared to the original condition from manufacturer.
If I loaded lab2 code and run it from the CCS Debugger, the Launchpad board worked just fine as it should even after I stopped the Debugger but still connected it to the computer USB port. However, if I did a hard reset or hardware reset, then the thing stopped working unless I start another Debugger section.
So I tried to program the board using LM flash programmer with lab2.bin file generated by CCS IDE. Everything went well with the flash programming process, but the Launchpad board still did nothing even after a hard reset. If I run the blank check on the LM flash programmer, it reported that the MCU is not blank.
I've looked around to find the cause of this problem, but have not found anything yet. Did anyone experience the same problem or have any ideas what might cause the problem. Any inputs/suggestions are greatly appreciated. Thanks in advance and have a wonderful day.
Best Regards,
TLN