Other Parts Discussed in Thread: TM4C1294NCZAD
Using the driverlib for Tiva TM4C1294NCZAD, I see the following lines of code starting at line 69:
//*****************************************************************************
//
// This is a mapping between interrupt number and the register that contains
// the priority encoding for that interrupt.
//
//*****************************************************************************
static const uint32_t g_pui32Regs[] =
{
0, NVIC_SYS_PRI1, NVIC_SYS_PRI2, NVIC_SYS_PRI3,
NVIC_PRI0, NVIC_PRI1,
NVIC_PRI2, NVIC_PRI3, NVIC_PRI4, NVIC_PRI5, NVIC_PRI6, NVIC_PRI7,
NVIC_PRI8, NVIC_PRI9, NVIC_PRI10, NVIC_PRI11, NVIC_PRI12, NVIC_PRI13,
NVIC_PRI14, NVIC_PRI15, NVIC_PRI16, NVIC_PRI17, NVIC_PRI18, NVIC_PRI19,
NVIC_PRI20, NVIC_PRI21, NVIC_PRI22, NVIC_PRI23, NVIC_PRI24, NVIC_PRI25,
NVIC_PRI26, NVIC_PRI27, NVIC_PRI28, NVIC_PRI29, NVIC_PRI30, NVIC_PRI31,
NVIC_PRI32, NVIC_PRI33, NVIC_PRI34
};
I believe that the line immediately following the left brace should NOT be there since it offsets all of the priority addresses. Has anyone else seen this or has it been fixed already or am I all wet?
Thanks,
Gary