This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tm4c1294 Ncpdt -fpga interface problem



Hello,

We have two pins to use as an interface between FPGA-TIVA.Actually for interrupt handling otherwisw before controller is up fpga is sending out its data.So we want to configure pins and probe them and se.The options we tried are

1).Port k pin 4

SYSCTL_RCGCGPIO_R |= (0x1 << 9); // Port k
GPIO_PORTK_DIR_R = 0X10;
GPIO_PORTK_DEN_R = 0X10;
GPIO_PORTK_DR4R_R = 0x10;
GPIO_PORTK_DATA_R=0X10;

2)port n pin 5

GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_5); // PB3(2) -> EN_GATE
GPIOPadConfigSet(GPIO_PORTN_BASE, GPIO_PIN_5, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
GPIODirModeSet (GPIO_PORTN_BASE, 0x20, GPIO_DIR_MODE_HW );
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_5, GPIO_PIN_5);

3)

MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_5, (MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_5)));

but we are not succeeding .We need the initial state of pin and configured output state to be different .(probing to virw difference)

Help for solutions.

Thankingyou,

Krishnan