This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC Sample code is stuck i While loop waiting for the conversion



Hello,

I'm using a TM4C1294 lauchpad and i was trying to get the adc running with the sample code single_ended.c in the Peripheral library. The only changes i made was change the GPIO pin to 0 i.e GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0); and change the baudrate of uart i.e  UARTStdioConfig(0, 9600, 16000000); . 

This was working for a while, and now it just gets stuck in the while loop ->while(!ADCIntStatus(ADC0_BASE, 3, false)). 

I'm not able to figure out what might have caused it to stop working because atleast when it was working, i could read some junk data. 

No changes were made in the code than above mentioned. I even tried with another launchpad, and still it does not work.

My clock is set at -

SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);

Please help me out in this . Let me know if i'm missing something. Its just annoying because it was working with the same code sometime back.

Thanks in advance,

Pooja