This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C EPI-Fpga interface Problem.We are doing FPGA-EPI INTERFACE IN gpmode .



Hello,

We are using GPMODE fpga INTERFACE BETWEEN CONTROLLER AND FPGA. Controller PIN is made up using

GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_4, GPIO_PIN_4);
GPIOPinTypeGPIOOutput(GPIO_PORTK_BASE, GPIO_PIN_4);

But before this a glich is coming a( noise type signal) which FPGA IS IDENTIFING,WHY IS IT COMING,HOW CAN IT BE AVOIDED...................

Regards,

Krishnan

  • Hello Krishnan,

    Till the time the IO is configured the pad is an input. At the same time the FPGA is also an input/ So there is a floating wire which can get coupled to any other trace in the proximity. The simplest solution is to have a Pull Down or Pull Up external to the devices and on the board. Also this is very much dependent on the type of noise that you are seeing.

    Regards
    Amit