This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Default speed Tiva C launchpad mcu

Genius 3300 points

Other Parts Discussed in Thread: TM4C123GH6PM

I am learning Tiva C series TM4C123GH6PM on launcpad.

What is default clock of MCU. isn't it 16Mhz?

But when I read SystemCoreClockUpdate() function it shows 12Mhz.

I have disabled clock_setup in system_TM4C.c file.

Code is attached for reference. it is using Keil5.

V1 basic.rar

  • Hello Vindhyachal,

    For a erased device it should be at least ~25MHz for USB Boot Loader to work with an external crystal. If the device has a program in it which does not configure the clocks then the frequency shall be PIOSC which is 16MHz

    Regards
    Amit
  • Hello Amit,

    The file I am using is attached. This is provided by keil.
    I haven't configure the clock i.e default clock is used.
    But when I had called the "SystemCoreClockUpdate()" , available "SystemCoreClock" get update to 12000000 i.e 12Mhz.

    In this file, below defination is given, is it wrong;

    #define XTALI (12000000UL) /* Internal oscillator freq */

    /**************************************************************************//**
     * @file     system_TM4C.c
     * @brief    CMSIS Device System Source File for
     *           Texas Instruments TIVA TM4C123 Device Series
     * @version  V1.00
     * @date     27. March 2013
     *
     * @note
     *                                                             modified by Keil
     ******************************************************************************/
    
    #include "stdint.h"
    #include "TM4C123.h"
    
    
    /*----------------------------------------------------------------------------
      DEFINES
     *----------------------------------------------------------------------------*/
    //-------- <<< Use Configuration Wizard in Context Menu >>> ------------------
    //
    // This file can be used by the Keil uVision configuration wizard to set
    // the following system clock configuration values.  Or the value of the
    // macros can be directly edited below if not using the uVision configuration
    // wizard.
    //
    //--------------------- Clock Configuration ----------------------------------
    //
    //  <e> Clock Configuration
    //          <i> Uncheck this box to skip the clock configuration.
    //
    // The following controls whether the system clock is configured in the
    // SystemInit() function.  If it is defined to be 1 then the system clock
    // will be configured according to the macros in the rest of this file.
    // If it is defined to be 0, then the system clock configuration is bypassed.
    //
    #define CLOCK_SETUP 1
    
    //********************************* RCC ***************************************
    //
    //  <h> Run-Mode Clock Configuration (RCC)
    
    //      <o> SYSDIV: System Clock Divisor <2-16>
    //          <i> Specifies the divisor used to generate the system clock from
    //          <i> either the PLL output of 200 MHz, or the chosen oscillator.
    //
    // The following value is the system clock divisor.  This will be applied if
    // USESYSDIV (see below) is enabled.  The valid range of dividers is 2-16.
    //
    #define CFG_RCC_SYSDIV 4
    
    //      <q> USESYSDIV: Enable System Clock Divider
    //          <i> Check this box to use the System Clock Divider
    //
    // The following controls whether the system clock divider is used.  If the
    // value is 1, then the system clock divider is used, and the value of the
    // system divider is defined by SYSDIV (see above).  If the value is 0, then
    // the system clock divider is not used.
    //
    #define CFG_RCC_USESYSDIV 1
    
    //      <q> USEPWMDIV: Enable PWM Clock Divider
    //          <i> Check this box to use the PWM Clock Divider
    //
    // The following controls whether the PWM clock divider is used.  If the
    // value is 1, then the PWM clock divider is used, and the value of the
    // PWM divider is defined by PWMDIV (see below).  If the value is 0, then
    // the PWM clock divider is not used.
    //
    #define CFG_RCC_USEPWMDIV 1
    
    //      <o> PWMDIV: PWM Unit Clock Divisor
    //              <0=> 0: SysClk / 2
    //              <1=> 1: SysClk / 4
    //              <2=> 2: SysClk / 8
    //              <3=> 3: SysClk / 16
    //              <4=> 4: SysClk / 32
    //              <5=> 5: SysClk / 64
    //              <6=> 6: SysClk / 64
    //              <7=> 7: SysClk / 64 (default)
    //          <i> Specifies the divisor used to generate the PWM time base,
    //          <i> from the System Clock
    //
    // The following value determines the PWM clock divider.  It is used if
    // USEPWMDIV is enabled (see above).  Otherwise the PWM clock is the same as
    // the system clock.  The value of the divider is determined by the table
    // above.
    //
    #define CFG_RCC_PWMDIV 7
    
    //      <q> PWRDN: PLL Power Down
    //          <i> Check this box to disable the PLL.  You must also choose
    //          <i> PLL Bypass.
    //
    // If the following value is 1, then the PLL is powered down.  Keep this value
    // as 1 if you do not need to use the PLL.  In this case, BYPASS (see below)
    // must also be set to 1.  If you are using the PLL, then this value must be
    // set to 0.
    //
    #define CFG_RCC_PWRDN 0
    
    //      <q> BYPASS: PLL Bypass
    //          <i> Check this box to not use the PLL for the System Clock
    //
    // Set the following value to 1 to bypass the PLL and not use it for the
    // system clock.  You must set this to 1 if PWRDN (above) is set to 1.  Set
    // this to 0 if you are using the PLL.
    //
    #define CFG_RCC_BYPASS 0
    
    //      <o> XTAL: Crystal Value
    //              < 0=>  0: 1.0000 MHz  (can not be used with PLL)
    //              < 1=>  1: 1.8432 MHz  (can not be used with PLL)
    //              < 2=>  2: 2.0000 MHz  (can not be used with PLL)
    //              < 3=>  3: 2.4576 MHz  (can not be used with PLL)
    //              < 4=>  4: 3.579545 MHz
    //              < 5=>  5: 3.6864 MHz
    //              < 6=>  6: 4.0000 MHz
    //              < 7=>  7: 4.096 MHz
    //              < 8=>  8: 4.9152 MHz
    //              < 9=>  9: 5.0000 MHz
    //              <10=> 10: 5.12 MHz
    //              <11=> 11: 6.0000 MHz (default)
    //              <12=> 12: 6.144 MHz
    //              <13=> 13: 7.3728 MHz
    //              <14=> 14: 8.0000 MHz
    //              <15=> 15: 8.192 MHz
    //              <16=> 16: 10.0 MHz
    //              <17=> 17: 12.0 MHz
    //              <18=> 18: 12.288 MHz
    //              <19=> 19: 13.56 MHz
    //              <20=> 20: 14.31818 MHz
    //              <21=> 21: 16.0 MHz
    //              <22=> 22: 16.384 MHz
    //          <i> This is the crystal frequency used for the main oscillator
    //
    // This value defines the crystal frequency for the main oscillator, according
    // to the table in the comments above.  If an external crystal is used, then
    // this value must be set to match the value of the crystal.
    //
    #define CFG_RCC_XTAL 21
    
    //      <o> OSCSRC: Oscillator Source
    //              <0=> 0: MOSC Main oscillator
    //              <1=> 1: IOSC Internal oscillator (default)
    //              <2=> 2: IOSC/4 Internal oscillator / 4 (this is necessary if used as input to PLL)
    //              <3=> 3: 30kHz 30-KHz internal oscillator
    //          <i> Chooses the oscillator that is used for the system clock,
    //          <i> or the PLL input.
    //
    // The following value chooses the oscillator source according to the table in
    // the comments above.
    //
    #define CFG_RCC_OSCSRC 0
    
    //      <q> IOSCDIS: Internal Oscillator Disable
    //          <i> Check this box to turn off the internal oscillator
    //
    // Set the following value to 1 to turn off the internal oscillator.  This
    // value can be set to 1 if you are not using the internal oscillator.
    //
    #define CFG_RCC_IOSCDIS 1
    
    //      <q> MOSCDIS: Main Oscillator Disable
    //          <i> Check this box to turn off the main oscillator
    //
    // Set the following value to 1 to turn off the main oscillator.  This
    // value can be set to 1 if you are not using the main oscillator.
    //
    #define CFG_RCC_MOSCDIS 0
    
    //  </h>
    
    //********************************* RCC2 **************************************
    //
    //   <h> Run-Mode Clock Configuration 2 (RCC2)
    
    //      <q> USERCC2: Use RCC2
    //          <i> Check this box to override some fields in RCC.  RCC2 provides
    //          <i> more bits for the system clock divider, and provides an
    //          <i> additional oscillator source.  If you do not need these
    //          <i> additional features, then leave this box unchecked.
    //
    // Set the following value to 1 to use the RCC2 register.  The RCC2 register
    // overrides some of the fields in the RCC register if it is used.
    //
    #define CFG_RCC2_USERCC2 0
    
    //      <o> SYSDIV2: System Clock Divisor <2-64>
    //          <i> Specifies the divisor used to generate the system clock from
    //          <i> either the PLL output of 200 MHz, or the oscillator.
    //
    // The following value is the system clock divisor.  This will be applied if
    // USESYSDIV in RCC is enabled.  The valid range of dividers is 2-64.
    //
    #define CFG_RCC_SYSDIV2 4
    
    //      <q> PWRDN2: Power Down PLL
    //          <i> Check this box to disable the PLL.  You must also choose
    //          <i> PLL Bypass.
    //
    // If the following value is 1, then the PLL is powered down.  Keep this value
    // as 1 if you do not need to use the PLL.  In this case, BYPASS2 (see below)
    // must also be set to 1.  If you are using the PLL, then this value must be
    // set to 0.
    //
    #define CFG_RCC_PWRDN2 0
    
    //      <q> BYPASS2: Bypass PLL
    //          <i> Check this box to not use the PLL for the System Clock
    //
    // Set the following value to 1 to bypass the PLL and not use it for the
    // system clock.  You must set this to 1 if PWRDN2 (above) is set to 1.  Set
    // this to 0 if you are using the PLL.
    //
    #define CFG_RCC_BYPASS2 0
    
    //      <o> OSCSRC2: Oscillator Source
    //              <0=> 0: MOSC Main oscillator
    //              <1=> 1: IOSC Internal oscillator (default)
    //              <2=> 2: IOSC/4 Internal oscillator / 4 (this is necessary if used as input to PLL)
    //              <3=> 3: 30kHz 30-kHz internal oscillator
    //              <7=> 7: 32kHz 32.768-kHz external oscillator
    //          <i> The oscillator that is used for the system clock, or the PLL input.
    //
    // The following value chooses the oscillator source according to the table in
    // the comments above.
    //
    #define CFG_RCC_OSCSRC2 0
    
    //  </h>
    //
    //  </e>
    
    //-------- <<< end of configuration section >>> ------------------------------
    
    //
    // The following macros are used to program the RCC and RCC2 registers in
    // the SystemInit() function.  Edit the macros above to change these values.
    //
    #define RCC_Val                                                               \
    (                                                                             \
        ((CFG_RCC_SYSDIV - 1)   << 23) |                                          \
        (CFG_RCC_USESYSDIV      << 22) |                                          \
        (CFG_RCC_USEPWMDIV      << 20) |                                          \
        (CFG_RCC_PWMDIV         << 17) |                                          \
        (CFG_RCC_PWRDN          << 13) |                                          \
        (CFG_RCC_BYPASS         << 11) |                                          \
        (CFG_RCC_XTAL           << 6)  |                                          \
        (CFG_RCC_OSCSRC         << 4)  |                                          \
        (CFG_RCC_IOSCDIS        << 1)  |                                          \
        (CFG_RCC_MOSCDIS        << 1)\
    )
    
    #define RCC2_Val                                                              \
    (                                                                             \
        (CFG_RCC2_USERCC2      << 31) |                                           \
        ((CFG_RCC_SYSDIV2 - 1)  << 23) |                                          \
        (CFG_RCC_PWRDN2         << 13) |                                          \
        (CFG_RCC_BYPASS2        << 11) |                                          \
        (CFG_RCC_OSCSRC2        << 4)\
    )
    
    
    /*----------------------------------------------------------------------------
      Define clocks
     *----------------------------------------------------------------------------*/
    #define XTALM       (16000000UL)            /* Main         oscillator freq */
    #define XTALI       (12000000UL)            /* Internal     oscillator freq */
    #define XTAL30K     (   30000UL)            /* Internal 30K oscillator freq */
    #define XTAL32K     (   32768UL)            /* external 32K oscillator freq */
    
    #define PLL_CLK    (400000000UL)
    #define ADC_CLK     (PLL_CLK/25)
    #define CAN_CLK     (PLL_CLK/50)
    
     /* Determine clock frequency according to clock register values */
      #if (RCC2_Val & (1UL<<31))                              /* is rcc2 used ? */
        #if (RCC2_Val & (1UL<<11))                           /* check BYPASS */
                  #if   (((RCC2_Val>>4) & 0x07) == 0x0)
                    #if   (((RCC_Val>>6) & 0x1F) == 0x0)
                          #define __CORE_CLK_PRE  1000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x1)
                          #define __CORE_CLK_PRE  1843200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x2)
                          #define __CORE_CLK_PRE  2000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x3)
                          #define __CORE_CLK_PRE  2457600UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x4)
                          #define __CORE_CLK_PRE  3579545UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x5)
                          #define __CORE_CLK_PRE  3686400UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x6)
                          #define __CORE_CLK_PRE  4000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x7)
                          #define __CORE_CLK_PRE  4096000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x8)
                          #define __CORE_CLK_PRE  4915200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x9)
                          #define __CORE_CLK_PRE  5000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xA)
                          #define __CORE_CLK_PRE  5120000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xB)
                          #define __CORE_CLK_PRE  6000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xC)
                          #define __CORE_CLK_PRE  6144000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xD)
                          #define __CORE_CLK_PRE  7372800UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xE)
                          #define __CORE_CLK_PRE  8000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xF)
                          #define __CORE_CLK_PRE  8192000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x10)
                          #define __CORE_CLK_PRE  10000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x11)
                          #define __CORE_CLK_PRE  12000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x12)
                          #define __CORE_CLK_PRE  12288000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x13)
                          #define __CORE_CLK_PRE  13560000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x14)
                          #define __CORE_CLK_PRE  14318180UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x15)
                          #define __CORE_CLK_PRE  16000000UL
                    #else
                          #define __CORE_CLK_PRE  16384000UL
                    #endif
                  #elif (((RCC2_Val>>4) & 0x07) == 0x1)
                      #define __CORE_CLK_PRE  XTALI
                  #elif (((RCC2_Val>>4) & 0x07) == 0x2)
                      #define __CORE_CLK_PRE  (XTALI/4)
                  #else
                      #define __CORE_CLK_PRE  XTAL30K
                  #endif
        #else
          #define __CORE_CLK_PRE   PLL_CLK
        #endif
        #if (RCC_Val & (1UL<<22))                            /* check USESYSDIV */
          #if (RCC2_Val & (1UL<<11))
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC2_Val>>23) & (0x3F)) + 1))
          #else
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC2_Val>>23) & (0x3F)) + 1) / 2)
          #endif
        #else
          #define __CORE_CLK  __CORE_CLK_PRE
        #endif
      #else
        #if (RCC_Val & (1UL<<11))                           /* check BYPASS */
                  #if   (((RCC_Val>>4) & 0x03) == 0x0)
                    #if   (((RCC_Val>>6) & 0x1F) == 0x0)
                          #define __CORE_CLK_PRE  1000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x1)
                          #define __CORE_CLK_PRE  1843200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x2)
                          #define __CORE_CLK_PRE  2000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x3)
                          #define __CORE_CLK_PRE  2457600UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x4)
                          #define __CORE_CLK_PRE  3579545UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x5)
                          #define __CORE_CLK_PRE  3686400UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x6)
                          #define __CORE_CLK_PRE  4000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x7)
                          #define __CORE_CLK_PRE  4096000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x8)
                          #define __CORE_CLK_PRE  4915200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x9)
                          #define __CORE_CLK_PRE  5000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xA)
                          #define __CORE_CLK_PRE  5120000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xB)
                          #define __CORE_CLK_PRE  6000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xC)
                          #define __CORE_CLK_PRE  6144000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xD)
                          #define __CORE_CLK_PRE  7372800UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xE)
                          #define __CORE_CLK_PRE  8000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xF)
                          #define __CORE_CLK_PRE  8192000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x10)
                          #define __CORE_CLK_PRE  10000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x11)
                          #define __CORE_CLK_PRE  12000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x12)
                          #define __CORE_CLK_PRE  12288000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x13)
                          #define __CORE_CLK_PRE  13560000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x14)
                          #define __CORE_CLK_PRE  14318180UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x15)
                          #define __CORE_CLK_PRE  16000000UL
                    #else
                          #define __CORE_CLK_PRE  16384000UL
                    #endif
                  #elif (((RCC_Val>>4) & 0x03) == 0x1)
                      #define __CORE_CLK_PRE  XTALI
                  #elif (((RCC_Val>>4) & 0x03) == 0x2)
                      #define __CORE_CLK_PRE  (XTALI/4)
                  #else
                      #define __CORE_CLK_PRE  XTAL30K
                  #endif
        #else
          #define __CORE_CLK_PRE   PLL_CLK
        #endif
        #if (RCC_Val & (1UL<<22))                            /* check USESYSDIV */
          #if (RCC_Val & (1UL<<11))                          /* check BYPASS */
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC_Val>>23) & (0x0F)) + 1))
          #else
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC_Val>>23) & (0x0F)) + 1) / 2)
          #endif
        #else
          #define __CORE_CLK  __CORE_CLK_PRE
        #endif
      #endif
    
    
    /*----------------------------------------------------------------------------
      Clock Variable definitions
     *----------------------------------------------------------------------------*/
    uint32_t SystemCoreClock = __CORE_CLK;  /*!< System Clock Frequency (Core Clock)*/
    
    
    /*----------------------------------------------------------------------------
      Clock functions
     *----------------------------------------------------------------------------*/
    
    /*----------------------------------------------------------------------------
      Get the OSC clock
     *----------------------------------------------------------------------------*/
    __INLINE static uint32_t getOscClk (uint32_t xtal, uint32_t oscSrc) {
      uint32_t oscClk = XTALI;
    
      switch (oscSrc) {                      /* switch OSCSRC */
        case 0:                              /* MOSC Main oscillator */
          switch (xtal) {                    /* switch XTAL */
            case 0x0:
              oscClk = 1000000UL;
              break;
            case 0x1:
              oscClk = 1843200UL;
              break;
            case 0x2:
              oscClk = 2000000UL;
              break;
            case 0x3:
              oscClk = 2457600UL;
              break;
            case 0x4:
              oscClk = 3579545UL;
              break;
            case 0x5:
              oscClk = 3686400UL;
              break;
            case 0x6:
              oscClk = 4000000UL;
              break;
            case 0x7:
              oscClk = 4096000UL;
              break;
            case 0x8:
              oscClk = 4915200UL;
              break;
            case 0x9:
              oscClk = 5000000UL;
              break;
            case 0xA:
              oscClk = 5120000UL;
              break;
            case 0xB:
              oscClk = 6000000UL;
              break;
            case 0xC:
              oscClk = 6144000UL;
              break;
            case 0xD:
              oscClk = 7372800UL;
              break;
            case 0xE:
              oscClk = 8000000UL;
              break;
            case 0xF:
              oscClk = 8192000UL;
              break;
            case 0x10:
              oscClk = 10000000UL;
              break;
            case 0x11:
              oscClk = 12000000UL;
              break;
            case 0x12:
              oscClk = 12288000UL;
              break;
            case 0x13:
              oscClk = 13560000UL;
              break;
            case 0x14:
              oscClk = 14318180UL;
              break;
            case 0x15:
              oscClk = 16000000UL;
              break;
            case 0x16:
              oscClk = 16384000UL;
              break;
           }
          break;
        case 1:                         /* IOSC Internal oscillator */
          oscClk = XTALI;
          break;
        case 2:                         /* IOSC/4 Internal oscillator/4 */
          oscClk = XTALI/4;
          break;
        case 3:                         /* 30kHz internal oscillator  */
          oscClk = XTAL30K;
          break;
      }
    
      return oscClk;
    }
    
    void SystemCoreClockUpdate (void)            /* Get Core Clock Frequency      */
    {
        uint32_t rcc, rcc2;
    
        /* Determine clock frequency according to clock register values */
        rcc  = SYSCTL->RCC;
        rcc2 = SYSCTL->RCC2;
    
      //if (rcc2 & SYSCTL_RCC2_USERCC2)
        if (rcc2 & (1UL<<31)) {                             /* is rcc2 is used ? */
      //  if (rcc2 & SYSCTL_RCC2_BYPASS2)
          if (rcc2 & (1UL<<11)) {                           /* check BYPASS */
            SystemCoreClock = getOscClk (((rcc>>6) & 0x0F),((rcc2>>4) & 0x07));
          } else {
            SystemCoreClock = PLL_CLK;
          }
          if (rcc & (1UL<<22)) {                            /* check USESYSDIV */
            if (rcc2 & (1UL<<11)) {
              SystemCoreClock = SystemCoreClock / (((rcc2>>23) & (0x3F)) + 1);
            } else {
              SystemCoreClock = SystemCoreClock / (((rcc2>>23) & (0x3F)) + 1) / 2;
            }
          }
        } else {
      //    if (RCC_Val & (1UL<<11)) {                            /* check BYPASS */
          if (rcc & (1UL<<11)) {                            /* check BYPASS */ /* Simulation does not work at this point */
            SystemCoreClock = getOscClk (((rcc>>6) & 0x1F),((rcc>>4) & 0x03));
          } else {
            SystemCoreClock = PLL_CLK;
          }
      //  if (rcc & SYSCTL_RCC_USE_SYSDIV)
          if (rcc & (1UL<<22)) {                            /* check USESYSDIV */
      //    if (rcc2 & SYSCTL_RCC_BYPASS)
            if (rcc & (1UL<<11)) {                          /* check BYPASS */ /* Simulation does not work at this point */
      //      if (RCC_Val & (1UL<<11)) {                          /* check BYPASS */
              SystemCoreClock = SystemCoreClock / (((rcc>>23) & (0x0F)) + 1);
            } else {
              SystemCoreClock = SystemCoreClock / (((rcc>>23) & (0x0F)) + 1) / 2;
            }
          }
        }
    }
    
    /**
     * Initialize the system
     *
     * @param  none
     * @return none
     *
     * @brief  Setup the microcontroller system.
     *         Initialize the System.
     */
    void SystemInit (void)
    {
    #if(CLOCK_SETUP)
        uint32_t i;
    #endif
    
      /* FPU settings ------------------------------------------------------------*/
      #if (__FPU_USED == 1)
        SCB->CPACR |= ((3UL << 10*2) |                 /* set CP10 Full Access */
                       (3UL << 11*2)  );               /* set CP11 Full Access */
      #endif
    
    #if(CLOCK_SETUP)
        SYSCTL->RCC2 = 0x07802810;    /* set default value */
        SYSCTL->RCC  = 0x078E3AD1;    /* set default value */
    
        SYSCTL->RCC  = (RCC_Val  | (1UL<<11) | (1UL<<13)) & ~(1UL<<22); /* set value with BYPASS, PWRDN set, USESYSDIV reset */
        SYSCTL->RCC2 = (RCC2_Val | (1UL<<11) | (1UL<<13));              /* set value with BYPASS, PWRDN set */
        for (i = 0; i < 1000; i++);   /* wait a while */
    
        SYSCTL->RCC  = (RCC_Val  | (1UL<<11)) & ~(1UL<<22);             /* set value with BYPASS, USESYSDIV reset */
        SYSCTL->RCC2 = (RCC2_Val | (1UL<<11));                          /* set value with BYPASS */
        for (i = 0; i < 1000; i++);   /* wait a while */
    
        SYSCTL->RCC  = (RCC_Val  | (1<<11));                            /* set value with BYPASS */
    
        if ( (((RCC_Val  & (1UL<<13)) == 0) && ((RCC2_Val & (1UL<<31)) == 0)) ||
             (((RCC2_Val & (1UL<<13)) == 0) && ((RCC2_Val & (1UL<<31)) != 0))   ) {
          while ((SYSCTL->RIS & (1UL<<6)) != (1UL<<6));                 /* wait until PLL is locked */
        }
    
        SYSCTL->RCC  = (RCC_Val);                                       /* set value */
        SYSCTL->RCC2 = (RCC2_Val);                                      /* set value */
        for (i = 0; i < 10000; i++);   /* wait a while */
    
    #endif
    }
    

  • Hello Vindhyachal,

    I think that is a definition from a LM3S part. You would need to modify it for 16MHz for the internal PIOSC.

    Regards
    Amit