This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Writing RCC & RCC2 TM4C123GH6PM

Genius 3300 points

Page 219 of  TM4C123GH6PM datasheet says 

Write the RCC register prior to writing the RCC2 register. If a subsequent write to the
RCC register is required, include another register access after writing the RCC register
and before writing the RCC2 register.

 

1. But system_TM4C.c file, as in code I have in another post(http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/406545)

Function SystemInit(), first write RCC2 & then RCC. is it worng there?

2. This line " include another register access", what access to another register. E.g if I have to write RCC register again what steps should I follow. is it:

RCC = x;

RCC2 = y;

RCC = z;

a = RCC;

RCC2 = b;

  • Hello Vindhyachal,

    I am not sure what source you are referring to in the SystemInit, but I would suggest importing the functionally correct SysCtlClockSet from TivaWare. Programming the TM4C123 clock is not a major activity, but not knowing the correct sequence may create a system deadlock.

    Regards
    Amit
  • I am using the file as I have attached. I have taken it from keil examples.

    /**************************************************************************//**
     * @file     system_TM4C.c
     * @brief    CMSIS Device System Source File for
     *           Texas Instruments TIVA TM4C123 Device Series
     * @version  V1.00
     * @date     27. March 2013
     *
     * @note
     *                                                             modified by Keil
     ******************************************************************************/
    
    #include "stdint.h"
    #include "TM4C123.h"
    
    
    /*----------------------------------------------------------------------------
      DEFINES
     *----------------------------------------------------------------------------*/
    //-------- <<< Use Configuration Wizard in Context Menu >>> ------------------
    //
    // This file can be used by the Keil uVision configuration wizard to set
    // the following system clock configuration values.  Or the value of the
    // macros can be directly edited below if not using the uVision configuration
    // wizard.
    //
    //--------------------- Clock Configuration ----------------------------------
    //
    //  <e> Clock Configuration
    //          <i> Uncheck this box to skip the clock configuration.
    //
    // The following controls whether the system clock is configured in the
    // SystemInit() function.  If it is defined to be 1 then the system clock
    // will be configured according to the macros in the rest of this file.
    // If it is defined to be 0, then the system clock configuration is bypassed.
    //
    #define CLOCK_SETUP 1
    
    //********************************* RCC ***************************************
    //
    //  <h> Run-Mode Clock Configuration (RCC)
    
    //      <o> SYSDIV: System Clock Divisor <2-16>
    //          <i> Specifies the divisor used to generate the system clock from
    //          <i> either the PLL output of 200 MHz, or the chosen oscillator.
    //
    // The following value is the system clock divisor.  This will be applied if
    // USESYSDIV (see below) is enabled.  The valid range of dividers is 2-16.
    //
    #define CFG_RCC_SYSDIV 4
    
    //      <q> USESYSDIV: Enable System Clock Divider
    //          <i> Check this box to use the System Clock Divider
    //
    // The following controls whether the system clock divider is used.  If the
    // value is 1, then the system clock divider is used, and the value of the
    // system divider is defined by SYSDIV (see above).  If the value is 0, then
    // the system clock divider is not used.
    //
    #define CFG_RCC_USESYSDIV 1
    
    //      <q> USEPWMDIV: Enable PWM Clock Divider
    //          <i> Check this box to use the PWM Clock Divider
    //
    // The following controls whether the PWM clock divider is used.  If the
    // value is 1, then the PWM clock divider is used, and the value of the
    // PWM divider is defined by PWMDIV (see below).  If the value is 0, then
    // the PWM clock divider is not used.
    //
    #define CFG_RCC_USEPWMDIV 1
    
    //      <o> PWMDIV: PWM Unit Clock Divisor
    //              <0=> 0: SysClk / 2
    //              <1=> 1: SysClk / 4
    //              <2=> 2: SysClk / 8
    //              <3=> 3: SysClk / 16
    //              <4=> 4: SysClk / 32
    //              <5=> 5: SysClk / 64
    //              <6=> 6: SysClk / 64
    //              <7=> 7: SysClk / 64 (default)
    //          <i> Specifies the divisor used to generate the PWM time base,
    //          <i> from the System Clock
    //
    // The following value determines the PWM clock divider.  It is used if
    // USEPWMDIV is enabled (see above).  Otherwise the PWM clock is the same as
    // the system clock.  The value of the divider is determined by the table
    // above.
    //
    #define CFG_RCC_PWMDIV 7
    
    //      <q> PWRDN: PLL Power Down
    //          <i> Check this box to disable the PLL.  You must also choose
    //          <i> PLL Bypass.
    //
    // If the following value is 1, then the PLL is powered down.  Keep this value
    // as 1 if you do not need to use the PLL.  In this case, BYPASS (see below)
    // must also be set to 1.  If you are using the PLL, then this value must be
    // set to 0.
    //
    #define CFG_RCC_PWRDN 0
    
    //      <q> BYPASS: PLL Bypass
    //          <i> Check this box to not use the PLL for the System Clock
    //
    // Set the following value to 1 to bypass the PLL and not use it for the
    // system clock.  You must set this to 1 if PWRDN (above) is set to 1.  Set
    // this to 0 if you are using the PLL.
    //
    #define CFG_RCC_BYPASS 0
    
    //      <o> XTAL: Crystal Value
    //              < 0=>  0: 1.0000 MHz  (can not be used with PLL)
    //              < 1=>  1: 1.8432 MHz  (can not be used with PLL)
    //              < 2=>  2: 2.0000 MHz  (can not be used with PLL)
    //              < 3=>  3: 2.4576 MHz  (can not be used with PLL)
    //              < 4=>  4: 3.579545 MHz
    //              < 5=>  5: 3.6864 MHz
    //              < 6=>  6: 4.0000 MHz
    //              < 7=>  7: 4.096 MHz
    //              < 8=>  8: 4.9152 MHz
    //              < 9=>  9: 5.0000 MHz
    //              <10=> 10: 5.12 MHz
    //              <11=> 11: 6.0000 MHz (default)
    //              <12=> 12: 6.144 MHz
    //              <13=> 13: 7.3728 MHz
    //              <14=> 14: 8.0000 MHz
    //              <15=> 15: 8.192 MHz
    //              <16=> 16: 10.0 MHz
    //              <17=> 17: 12.0 MHz
    //              <18=> 18: 12.288 MHz
    //              <19=> 19: 13.56 MHz
    //              <20=> 20: 14.31818 MHz
    //              <21=> 21: 16.0 MHz
    //              <22=> 22: 16.384 MHz
    //          <i> This is the crystal frequency used for the main oscillator
    //
    // This value defines the crystal frequency for the main oscillator, according
    // to the table in the comments above.  If an external crystal is used, then
    // this value must be set to match the value of the crystal.
    //
    #define CFG_RCC_XTAL 21
    
    //      <o> OSCSRC: Oscillator Source
    //              <0=> 0: MOSC Main oscillator
    //              <1=> 1: IOSC Internal oscillator (default)
    //              <2=> 2: IOSC/4 Internal oscillator / 4 (this is necessary if used as input to PLL)
    //              <3=> 3: 30kHz 30-KHz internal oscillator
    //          <i> Chooses the oscillator that is used for the system clock,
    //          <i> or the PLL input.
    //
    // The following value chooses the oscillator source according to the table in
    // the comments above.
    //
    #define CFG_RCC_OSCSRC 0
    
    //      <q> IOSCDIS: Internal Oscillator Disable
    //          <i> Check this box to turn off the internal oscillator
    //
    // Set the following value to 1 to turn off the internal oscillator.  This
    // value can be set to 1 if you are not using the internal oscillator.
    //
    #define CFG_RCC_IOSCDIS 1
    
    //      <q> MOSCDIS: Main Oscillator Disable
    //          <i> Check this box to turn off the main oscillator
    //
    // Set the following value to 1 to turn off the main oscillator.  This
    // value can be set to 1 if you are not using the main oscillator.
    //
    #define CFG_RCC_MOSCDIS 0
    
    //  </h>
    
    //********************************* RCC2 **************************************
    //
    //   <h> Run-Mode Clock Configuration 2 (RCC2)
    
    //      <q> USERCC2: Use RCC2
    //          <i> Check this box to override some fields in RCC.  RCC2 provides
    //          <i> more bits for the system clock divider, and provides an
    //          <i> additional oscillator source.  If you do not need these
    //          <i> additional features, then leave this box unchecked.
    //
    // Set the following value to 1 to use the RCC2 register.  The RCC2 register
    // overrides some of the fields in the RCC register if it is used.
    //
    #define CFG_RCC2_USERCC2 0
    
    //      <o> SYSDIV2: System Clock Divisor <2-64>
    //          <i> Specifies the divisor used to generate the system clock from
    //          <i> either the PLL output of 200 MHz, or the oscillator.
    //
    // The following value is the system clock divisor.  This will be applied if
    // USESYSDIV in RCC is enabled.  The valid range of dividers is 2-64.
    //
    #define CFG_RCC_SYSDIV2 4
    
    //      <q> PWRDN2: Power Down PLL
    //          <i> Check this box to disable the PLL.  You must also choose
    //          <i> PLL Bypass.
    //
    // If the following value is 1, then the PLL is powered down.  Keep this value
    // as 1 if you do not need to use the PLL.  In this case, BYPASS2 (see below)
    // must also be set to 1.  If you are using the PLL, then this value must be
    // set to 0.
    //
    #define CFG_RCC_PWRDN2 0
    
    //      <q> BYPASS2: Bypass PLL
    //          <i> Check this box to not use the PLL for the System Clock
    //
    // Set the following value to 1 to bypass the PLL and not use it for the
    // system clock.  You must set this to 1 if PWRDN2 (above) is set to 1.  Set
    // this to 0 if you are using the PLL.
    //
    #define CFG_RCC_BYPASS2 0
    
    //      <o> OSCSRC2: Oscillator Source
    //              <0=> 0: MOSC Main oscillator
    //              <1=> 1: IOSC Internal oscillator (default)
    //              <2=> 2: IOSC/4 Internal oscillator / 4 (this is necessary if used as input to PLL)
    //              <3=> 3: 30kHz 30-kHz internal oscillator
    //              <7=> 7: 32kHz 32.768-kHz external oscillator
    //          <i> The oscillator that is used for the system clock, or the PLL input.
    //
    // The following value chooses the oscillator source according to the table in
    // the comments above.
    //
    #define CFG_RCC_OSCSRC2 0
    
    //  </h>
    //
    //  </e>
    
    //-------- <<< end of configuration section >>> ------------------------------
    
    //
    // The following macros are used to program the RCC and RCC2 registers in
    // the SystemInit() function.  Edit the macros above to change these values.
    //
    #define RCC_Val                                                               \
    (                                                                             \
        ((CFG_RCC_SYSDIV - 1)   << 23) |                                          \
        (CFG_RCC_USESYSDIV      << 22) |                                          \
        (CFG_RCC_USEPWMDIV      << 20) |                                          \
        (CFG_RCC_PWMDIV         << 17) |                                          \
        (CFG_RCC_PWRDN          << 13) |                                          \
        (CFG_RCC_BYPASS         << 11) |                                          \
        (CFG_RCC_XTAL           << 6)  |                                          \
        (CFG_RCC_OSCSRC         << 4)  |                                          \
        (CFG_RCC_IOSCDIS        << 1)  |                                          \
        (CFG_RCC_MOSCDIS        << 1)\
    )
    
    #define RCC2_Val                                                              \
    (                                                                             \
        (CFG_RCC2_USERCC2      << 31) |                                           \
        ((CFG_RCC_SYSDIV2 - 1)  << 23) |                                          \
        (CFG_RCC_PWRDN2         << 13) |                                          \
        (CFG_RCC_BYPASS2        << 11) |                                          \
        (CFG_RCC_OSCSRC2        << 4)\
    )
    
    
    /*----------------------------------------------------------------------------
      Define clocks
     *----------------------------------------------------------------------------*/
    #define XTALM       (16000000UL)            /* Main         oscillator freq */
    #define XTALI       (12000000UL)            /* Internal     oscillator freq */
    #define XTAL30K     (   30000UL)            /* Internal 30K oscillator freq */
    #define XTAL32K     (   32768UL)            /* external 32K oscillator freq */
    
    #define PLL_CLK    (400000000UL)
    #define ADC_CLK     (PLL_CLK/25)
    #define CAN_CLK     (PLL_CLK/50)
    
     /* Determine clock frequency according to clock register values */
      #if (RCC2_Val & (1UL<<31))                              /* is rcc2 used ? */
        #if (RCC2_Val & (1UL<<11))                           /* check BYPASS */
                  #if   (((RCC2_Val>>4) & 0x07) == 0x0)
                    #if   (((RCC_Val>>6) & 0x1F) == 0x0)
                          #define __CORE_CLK_PRE  1000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x1)
                          #define __CORE_CLK_PRE  1843200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x2)
                          #define __CORE_CLK_PRE  2000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x3)
                          #define __CORE_CLK_PRE  2457600UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x4)
                          #define __CORE_CLK_PRE  3579545UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x5)
                          #define __CORE_CLK_PRE  3686400UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x6)
                          #define __CORE_CLK_PRE  4000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x7)
                          #define __CORE_CLK_PRE  4096000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x8)
                          #define __CORE_CLK_PRE  4915200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x9)
                          #define __CORE_CLK_PRE  5000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xA)
                          #define __CORE_CLK_PRE  5120000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xB)
                          #define __CORE_CLK_PRE  6000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xC)
                          #define __CORE_CLK_PRE  6144000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xD)
                          #define __CORE_CLK_PRE  7372800UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xE)
                          #define __CORE_CLK_PRE  8000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xF)
                          #define __CORE_CLK_PRE  8192000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x10)
                          #define __CORE_CLK_PRE  10000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x11)
                          #define __CORE_CLK_PRE  12000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x12)
                          #define __CORE_CLK_PRE  12288000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x13)
                          #define __CORE_CLK_PRE  13560000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x14)
                          #define __CORE_CLK_PRE  14318180UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x15)
                          #define __CORE_CLK_PRE  16000000UL
                    #else
                          #define __CORE_CLK_PRE  16384000UL
                    #endif
                  #elif (((RCC2_Val>>4) & 0x07) == 0x1)
                      #define __CORE_CLK_PRE  XTALI
                  #elif (((RCC2_Val>>4) & 0x07) == 0x2)
                      #define __CORE_CLK_PRE  (XTALI/4)
                  #else
                      #define __CORE_CLK_PRE  XTAL30K
                  #endif
        #else
          #define __CORE_CLK_PRE   PLL_CLK
        #endif
        #if (RCC_Val & (1UL<<22))                            /* check USESYSDIV */
          #if (RCC2_Val & (1UL<<11))
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC2_Val>>23) & (0x3F)) + 1))
          #else
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC2_Val>>23) & (0x3F)) + 1) / 2)
          #endif
        #else
          #define __CORE_CLK  __CORE_CLK_PRE
        #endif
      #else
        #if (RCC_Val & (1UL<<11))                           /* check BYPASS */
                  #if   (((RCC_Val>>4) & 0x03) == 0x0)
                    #if   (((RCC_Val>>6) & 0x1F) == 0x0)
                          #define __CORE_CLK_PRE  1000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x1)
                          #define __CORE_CLK_PRE  1843200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x2)
                          #define __CORE_CLK_PRE  2000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x3)
                          #define __CORE_CLK_PRE  2457600UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x4)
                          #define __CORE_CLK_PRE  3579545UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x5)
                          #define __CORE_CLK_PRE  3686400UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x6)
                          #define __CORE_CLK_PRE  4000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x7)
                          #define __CORE_CLK_PRE  4096000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x8)
                          #define __CORE_CLK_PRE  4915200UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x9)
                          #define __CORE_CLK_PRE  5000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xA)
                          #define __CORE_CLK_PRE  5120000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xB)
                          #define __CORE_CLK_PRE  6000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xC)
                          #define __CORE_CLK_PRE  6144000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xD)
                          #define __CORE_CLK_PRE  7372800UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xE)
                          #define __CORE_CLK_PRE  8000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0xF)
                          #define __CORE_CLK_PRE  8192000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x10)
                          #define __CORE_CLK_PRE  10000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x11)
                          #define __CORE_CLK_PRE  12000000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x12)
                          #define __CORE_CLK_PRE  12288000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x13)
                          #define __CORE_CLK_PRE  13560000UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x14)
                          #define __CORE_CLK_PRE  14318180UL
                    #elif (((RCC_Val>>6) & 0x1F) == 0x15)
                          #define __CORE_CLK_PRE  16000000UL
                    #else
                          #define __CORE_CLK_PRE  16384000UL
                    #endif
                  #elif (((RCC_Val>>4) & 0x03) == 0x1)
                      #define __CORE_CLK_PRE  XTALI
                  #elif (((RCC_Val>>4) & 0x03) == 0x2)
                      #define __CORE_CLK_PRE  (XTALI/4)
                  #else
                      #define __CORE_CLK_PRE  XTAL30K
                  #endif
        #else
          #define __CORE_CLK_PRE   PLL_CLK
        #endif
        #if (RCC_Val & (1UL<<22))                            /* check USESYSDIV */
          #if (RCC_Val & (1UL<<11))                          /* check BYPASS */
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC_Val>>23) & (0x0F)) + 1))
          #else
            #define __CORE_CLK  (__CORE_CLK_PRE / (((RCC_Val>>23) & (0x0F)) + 1) / 2)
          #endif
        #else
          #define __CORE_CLK  __CORE_CLK_PRE
        #endif
      #endif
    
    
    /*----------------------------------------------------------------------------
      Clock Variable definitions
     *----------------------------------------------------------------------------*/
    uint32_t SystemCoreClock = __CORE_CLK;  /*!< System Clock Frequency (Core Clock)*/
    
    
    /*----------------------------------------------------------------------------
      Clock functions
     *----------------------------------------------------------------------------*/
    
    /*----------------------------------------------------------------------------
      Get the OSC clock
     *----------------------------------------------------------------------------*/
    __INLINE static uint32_t getOscClk (uint32_t xtal, uint32_t oscSrc) {
      uint32_t oscClk = XTALI;
    
      switch (oscSrc) {                      /* switch OSCSRC */
        case 0:                              /* MOSC Main oscillator */
          switch (xtal) {                    /* switch XTAL */
            case 0x0:
              oscClk = 1000000UL;
              break;
            case 0x1:
              oscClk = 1843200UL;
              break;
            case 0x2:
              oscClk = 2000000UL;
              break;
            case 0x3:
              oscClk = 2457600UL;
              break;
            case 0x4:
              oscClk = 3579545UL;
              break;
            case 0x5:
              oscClk = 3686400UL;
              break;
            case 0x6:
              oscClk = 4000000UL;
              break;
            case 0x7:
              oscClk = 4096000UL;
              break;
            case 0x8:
              oscClk = 4915200UL;
              break;
            case 0x9:
              oscClk = 5000000UL;
              break;
            case 0xA:
              oscClk = 5120000UL;
              break;
            case 0xB:
              oscClk = 6000000UL;
              break;
            case 0xC:
              oscClk = 6144000UL;
              break;
            case 0xD:
              oscClk = 7372800UL;
              break;
            case 0xE:
              oscClk = 8000000UL;
              break;
            case 0xF:
              oscClk = 8192000UL;
              break;
            case 0x10:
              oscClk = 10000000UL;
              break;
            case 0x11:
              oscClk = 12000000UL;
              break;
            case 0x12:
              oscClk = 12288000UL;
              break;
            case 0x13:
              oscClk = 13560000UL;
              break;
            case 0x14:
              oscClk = 14318180UL;
              break;
            case 0x15:
              oscClk = 16000000UL;
              break;
            case 0x16:
              oscClk = 16384000UL;
              break;
           }
          break;
        case 1:                         /* IOSC Internal oscillator */
          oscClk = XTALI;
          break;
        case 2:                         /* IOSC/4 Internal oscillator/4 */
          oscClk = XTALI/4;
          break;
        case 3:                         /* 30kHz internal oscillator  */
          oscClk = XTAL30K;
          break;
      }
    
      return oscClk;
    }
    
    void SystemCoreClockUpdate (void)            /* Get Core Clock Frequency      */
    {
        uint32_t rcc, rcc2;
    
        /* Determine clock frequency according to clock register values */
        rcc  = SYSCTL->RCC;
        rcc2 = SYSCTL->RCC2;
    
      //if (rcc2 & SYSCTL_RCC2_USERCC2)
        if (rcc2 & (1UL<<31)) {                             /* is rcc2 is used ? */
      //  if (rcc2 & SYSCTL_RCC2_BYPASS2)
          if (rcc2 & (1UL<<11)) {                           /* check BYPASS */
            SystemCoreClock = getOscClk (((rcc>>6) & 0x0F),((rcc2>>4) & 0x07));
          } else {
            SystemCoreClock = PLL_CLK;
          }
          if (rcc & (1UL<<22)) {                            /* check USESYSDIV */
            if (rcc2 & (1UL<<11)) {
              SystemCoreClock = SystemCoreClock / (((rcc2>>23) & (0x3F)) + 1);
            } else {
              SystemCoreClock = SystemCoreClock / (((rcc2>>23) & (0x3F)) + 1) / 2;
            }
          }
        } else {
      //    if (RCC_Val & (1UL<<11)) {                            /* check BYPASS */
          if (rcc & (1UL<<11)) {                            /* check BYPASS */ /* Simulation does not work at this point */
            SystemCoreClock = getOscClk (((rcc>>6) & 0x1F),((rcc>>4) & 0x03));
          } else {
            SystemCoreClock = PLL_CLK;
          }
      //  if (rcc & SYSCTL_RCC_USE_SYSDIV)
          if (rcc & (1UL<<22)) {                            /* check USESYSDIV */
      //    if (rcc2 & SYSCTL_RCC_BYPASS)
            if (rcc & (1UL<<11)) {                          /* check BYPASS */ /* Simulation does not work at this point */
      //      if (RCC_Val & (1UL<<11)) {                          /* check BYPASS */
              SystemCoreClock = SystemCoreClock / (((rcc>>23) & (0x0F)) + 1);
            } else {
              SystemCoreClock = SystemCoreClock / (((rcc>>23) & (0x0F)) + 1) / 2;
            }
          }
        }
    }
    
    /**
     * Initialize the system
     *
     * @param  none
     * @return none
     *
     * @brief  Setup the microcontroller system.
     *         Initialize the System.
     */
    void SystemInit (void)
    {
    #if(CLOCK_SETUP)
        uint32_t i;
    #endif
    
      /* FPU settings ------------------------------------------------------------*/
      #if (__FPU_USED == 1)
        SCB->CPACR |= ((3UL << 10*2) |                 /* set CP10 Full Access */
                       (3UL << 11*2)  );               /* set CP11 Full Access */
      #endif
    
    #if(CLOCK_SETUP)
        SYSCTL->RCC2 = 0x07802810;    /* set default value */
        SYSCTL->RCC  = 0x078E3AD1;    /* set default value */
    
        SYSCTL->RCC  = (RCC_Val  | (1UL<<11) | (1UL<<13)) & ~(1UL<<22); /* set value with BYPASS, PWRDN set, USESYSDIV reset */
        SYSCTL->RCC2 = (RCC2_Val | (1UL<<11) | (1UL<<13));              /* set value with BYPASS, PWRDN set */
        for (i = 0; i < 1000; i++);   /* wait a while */
    
        SYSCTL->RCC  = (RCC_Val  | (1UL<<11)) & ~(1UL<<22);             /* set value with BYPASS, USESYSDIV reset */
        SYSCTL->RCC2 = (RCC2_Val | (1UL<<11));                          /* set value with BYPASS */
        for (i = 0; i < 1000; i++);   /* wait a while */
    
        SYSCTL->RCC  = (RCC_Val  | (1<<11));                            /* set value with BYPASS */
    
        if ( (((RCC_Val  & (1UL<<13)) == 0) && ((RCC2_Val & (1UL<<31)) == 0)) ||
             (((RCC2_Val & (1UL<<13)) == 0) && ((RCC2_Val & (1UL<<31)) != 0))   ) {
          while ((SYSCTL->RIS & (1UL<<6)) != (1UL<<6));                 /* wait until PLL is locked */
        }
    
        SYSCTL->RCC  = (RCC_Val);                                       /* set value */
        SYSCTL->RCC2 = (RCC2_Val);                                      /* set value */
        for (i = 0; i < 10000; i++);   /* wait a while */
    
    #endif
    }
    

  • Hello Vindhyachal,

    I see some issues in the file, e.g. the PIOSC default is kept at 12MHz whereas it is 16MHz. I would suggest importing the TivaWare API's to allow for the correct clock settings using SysCtlClockSet and SysCtlClockGet.

    Regards
    Amit
  • SysCtlClockSet and SysCtlClockGet do indeed work. But I have to say it is frustrating that you can't set up RCC and RCC2 using the data sheet if you want to go that route. The TivaWare routines have several extra delays that are not documented in the data sheet. And other delays that are implemented differently than suggested in the data sheet. Also, the routine doesn't seem to follow this confusing note:

    Important: Write the RCC register prior to writing the RCC2 register. If a subsequent write to the
    RCC register is required, include another register access after writing the RCC register
    and before writing the RCC2 register.

  • Hello Patrick,

    Setting up RCC and RCC2 for TM4C123 was never easy for me either. Took me time to understand and this was one feedback for improving the clock function for TM4C129.

    Regards
    Amit