Other Parts Discussed in Thread: TM4C123GH6PGE
Hi ,
i m using internal eeprom of the tm4c123gh6pge. when running the individually with break point, data is writing to the memory address. but when im integrating to my project code is stops at eepromprogram function. if i debud step by step its coming out from that function. im placing breakpoint also.
FlashErase(0x10010);
FlashProgram(pui32Data, 0x10010, sizeof(pui32Data));
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x02);
SysCtlDelay(SysCtlClockGet()/(100*3));
SysCtlPeripheralEnable(SYSCTL_PERIPH_EEPROM0);
EEPROMInit();
EEPROMMassErase();
EEPROMRead(pui32Read, 0x0, sizeof(pui32Read));
EEPROMProgram(pui32Data, 0x0, sizeof(pui32Data));
EEPROMRead(pui32Read, 0x0, sizeof(pui32Read));
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x04);