Other Parts Discussed in Thread: RM48L952
I am using the RM48 Hercules Development Kit, with a RM48l952 MCU .
I managed to transmite data in Single-Buffer Mode using SCI2(SCI/LIN module) interrupt mode .Now I want to change it into Multi-Buffer Mode .As
described in the mannual ,Multi-Buffer Mode is selected when MBUF MODE bit is 1.And the data to be transmitted has to be written to LINTD0 and LINTD1
register, based on the number of bytes.So I changed the programme as follows,but it didn't work. What should I do ?
#include "lin.h"
scilinREG->GCR1 = (1 << 25) /* enable transmit */
| (1 << 24) /* enable receive */
| (1 << 10) /* enable multi-buffer */
| (1 << 5) /* internal clock (device has no clock pin) */
| ((2-1) << 4) /* number of stop bits */
| (0 << 3) /* even parity, otherwise odd */
| (0 << 2) /* enable parity */
| (1 << 1); /* asynchronous timing mode */
void linHighLevelInterrupt(void)
case 12:
/* transmit */
//if(--g_sciTransfer[1].length > 0)
// {
// scilinREG->TD = *g_sciTransfer[1].data++;
// }
if (--g_sciTransfer[1].length > 0)
{
//scilinREG->TD = *g_sciTransfer[1].data++;
length = g_sciTransfer[1].length;
*pData = *g_sciTransfer[1].data + length;
for (i = length; i >= 0; i--)
{
linREG->TDx[i] = *pData--;
}
}
else
{
scilinREG->CLRINT = SCI_TX_INT;
sciNotification(scilinREG, SCI_TX_INT);
}
break;