I'm planning to purchase XDS560v2 PRO TRACE and use it to L952 HDK and my PWB including MIPI 60 connector.
But Some PWB of mine have only ARM 20 pin connector including no ETM. I want to use XDS560v2 PRO TRACE to the PWBs with L952ZWT and ARM 20 connector.
Also, I'm going to get an adapter for MIPI 60 to ARM 20.
I want to know functional differences between MIPI 60 and ARM 20 when using Trace Analyzer in CCSv6 (or CCSv5).
I guess there are some limitation in Receiver/Transport Settings.
Best Regards,
Satoshi Shinohara