Other Parts Discussed in Thread: TM4C1294NCPDT, TEST2
Hello
I tried to activate the System Exception Module for the FPU on a TM4C1294NCPDT. But it is just not entering the fault handler.
The IRQ is enabled via SysExcIntEnable(SYSEXC_INT_FP_DZC);
The fault handler is set in the startup file startup_rvmdk.S
Find attached the Project as zip file.
//*****************************************************************************
//
// The interrupt handler.
//
//*****************************************************************************
void FPU_Fault_Handler(void)
{
uint32_t ui32IntFlags;
ui32IntFlags = ROM_SysExcIntStatus(true);
ROM_SysExcIntClear(ui32IntFlags);
while(1)
{
}
}
//*****************************************************************************
//
// example
//
//*****************************************************************************
float test=0, test2;
int
main(void)
{
//
// Run from the PLL at 120 MHz.
//
MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
ROM_SysExcIntEnable(SYSEXC_INT_FP_DZC);
//
// Enable processor interrupts.
//
IntMasterEnable();
//
// Loop forever
//
while(1)
{
// devide by zero
test2 = 1.0f/test;
}
}