This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO pin configuration sequence tm4c123gh6pm

Genius 3300 points

Other Parts Discussed in Thread: TM4C123GH6PM

I have wrote GPIO configuration for tm4c123gh6pm. is below sequence correct. Does any additional register need to be configured or rest of GPIO registers are don't care for input & output

1. Pin as Input pull up

/* PF0 as input pull up */    
    SYSCTL->RCGCGPIO |= REG32_BIT_5;               /* enable PORTF clock */
    while(! (SYSCTL->PRGPIO & REG32_BIT_5));       /* while periph ready */
    SYSCTL->GPIOHBCTL |= REG32_BIT_5;              /* enable access to AHB bus  */
    
    GPIOF_AHB->LOCK      = 0x4c4f434bU;            /* write lock key */
    GPIOF_AHB->CR       |= REG32_BIT_0;            /* enable write to PF0 pin */ 
    
    GPIOF_AHB->DIR      &= (u32_t)(~REG32_BIT_0);  /* make as input */
    GPIOF_AHB->AFSEL    &= (u32_t)(~REG32_BIT_0);  /* used as GPIO */
    GPIOF_AHB->PUR      |= REG32_BIT_0;            /* pull up enabled */
    GPIOF_AHB->PDR      &= (u32_t)(~REG32_BIT_0);  /* pull down disabled */
    GPIOF_AHB->ODR      &= (u32_t)(~REG32_BIT_0);  /* not open drain */
    GPIOF_AHB->AMSEL    &= (u32_t)(~REG32_BIT_0);  /* analog function disabled */  
    GPIOF_AHB->DEN      |= REG32_BIT_0;            /* digital function enabled */

2. Pin as output

/* PF1 as output low */    
    SYSCTL->RCGCGPIO |= REG32_BIT_5;                /* enable PORTF clock */
    while(! (SYSCTL->PRGPIO & REG32_BIT_5));        /* while periph ready */
    SYSCTL->GPIOHBCTL |= REG32_BIT_5;               /* enable access to AHB bus  */

    GPIOF_AHB->DATA     &= (u32_t)(~REG32_BIT_1);  /* pin low on output */  
    GPIOF_AHB->DIR      |= REG32_BIT_1;            /* make as output */
    GPIOF_AHB->AFSEL    &= (u32_t)(~REG32_BIT_1);  /* used as GPIO */
    GPIOF_AHB->PUR      &= (u32_t)(~REG32_BIT_1);  /* pull up disabled */
    GPIOF_AHB->PDR      &= (u32_t)(~REG32_BIT_1);  /* pull down disabled */
    GPIOF_AHB->ODR      &= (u32_t)(~REG32_BIT_1);  /* not open drain */
    GPIOF_AHB->AMSEL    &= (u32_t)(~REG32_BIT_1);  /* analog function disabled */  
    GPIOF_AHB->DR8R     &= (u32_t)(~REG32_BIT_1);  /* 8mA drive disable */
    GPIOF_AHB->DR4R     &= (u32_t)(~REG32_BIT_1);  /* 4mA drive disable */    
    GPIOF_AHB->DR2R     |= REG32_BIT_1;            /* 2mA drive enable */
    GPIOF_AHB->SLR      &= (u32_t)(~REG32_BIT_1);  /* slew disabled */
    GPIOF_AHB->DEN      |= REG32_BIT_1;            /* digital function enabled */

3. What is slew control used for when drive is 8mA.