Other Parts Discussed in Thread: TM4C129XNCZAD, TM4C1292NCPDT, EK-TM4C1294XL
Hi Guys,
I have gone through many documentation and forum questions but since I'm a novice in this field I was not able to understand it and wanted your help regarding some doubts.
I have TM4C129XNCZAD and TM4C1292NCPDT micro controllers(not the development boards or eval boards)
I wanted to design my own custom board using any one of the above micro controllers (I still have not decided on the uC) so i would like to know
1) How do i program these micro controllers using UART and LM flash programmer (can i directly connect RX TX GND of serial port pins of my computer to the board and download? )
2) With respect to my above question will the fresh micro controller come with pre loaded serial( UART) boot loader so that it can download my application code on the flash or should I burn the serial (UART) boot loader(If yes through what interface? (JTAG?) and where will i get the serial (UART) boot loader?)
Thank you for your valuable time and effort
Regards
Sanjay Anand