Other Parts Discussed in Thread: LMFLASHPROGRAMMER
I would greatly appreciate help with a nasty problem: I have locked-up a TM4C123_LaunchPad connected via USB to my Windows PC (64 bit, Win7 Pro). The
IDE I am using is Keil uVision4. This happened while I was "experimenting" with configuring GPIO ports on the LaunchPad.
After spending all day today trying to sort this out I finally found Sue Cozart's TI E3E Community "JTAG Communication Failures" post (Dec 19, 2013 3:56 PM).
The item "2. Changing the function of the Port C[3:0] pins, which are muxed with the JTAG pins.", hit home as I was attempting to use PORTC. Once I loaded
the code with the PORTC configuration code, in to the LaunchPad it stopped communicating.
I have tried using the LM Flash Programmer with no success. Clicking the "Debug Port Unlock" in "Other Utilities" results in the following message: "**ERROR**
Failed to unlock connected device!". Clicking "Hardware" button in the "Program" tab results in: "**ERROR**: Cannot find target device". BYW, I don't have the
MAC address for the board as it's not communicating.
Part of my "experiment" program loaded and is partially working, the on-board green LED on PORTF cycles on-off when the reset button is pressed. However,
there is no output on pins on PORTB and PORTC. All the drivers are installed and were functioning prior to my "experiment"!
All help will be greatly appreciated.
Thanks, Bob