Other Parts Discussed in Thread: TM4C123GH6PM, EK-TM4C1294XL
I used the below program for UART0 and I got the output, but when i used the same program for other UART's by enabling the corresponding peripheral and its respective base im not getting output.
what could be the problem?
#include <stdint.h>
#include <stdbool.h>
#include <hw_memmap.h>
#include <hw_types.h>
#include <gpio.h>
#include <sysctl.h>
#include <uart.h>
int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(0x00000001);
GPIOPinConfigure(0x00000401);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200,(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
UARTEnable(UART0_BASE);
UARTCharPut(UART0_BASE, 'E');
UARTCharPut(UART0_BASE, 'n');
UARTCharPut(UART0_BASE, 't');
UARTCharPut(UART0_BASE, 'e');
UARTCharPut(UART0_BASE, 'r');
UARTCharPut(UART0_BASE, ' ');
UARTCharPut(UART0_BASE, 'T');
UARTCharPut(UART0_BASE, 'e');
UARTCharPut(UART0_BASE, 'x');
UARTCharPut(UART0_BASE, 't');
UARTCharPut(UART0_BASE, ':');
UARTCharPut(UART0_BASE, ' ');
while (1)
{
if(UARTCharsAvail(UART0_BASE)) UARTCharPut(UART0_BASE, UARTCharGet(UART0_BASE));
}
}