Other Parts Discussed in Thread: TMS570LS3137
Hey guys,
we need some information regarding the STC test feature of the TMS570LS3137.
When preparing the SoC to perform the STC test, a WFI (wait for interrupt) instruction is supposed to start the test and put the CPU in a low-power mode. When the test is running, a CPU reset is expected when the test has finished.
Now, as far as I know, any interrupt (in addition to a reset) can wake up the CPU from this low-power (WFI) mode.
2 Questions are therefore from interest:
- What will happen to the STC test, if the CPU get woken up by any interrupt during the test operation?
- Will the expected CPU reset by asserted either never or at some later point in time?
Thanks in advance.
Kind regards,
Michael