Other Parts Discussed in Thread: HALCOGEN, UNIFLASH
Hello TI,
I am using CCS v6.1.0.00104 on TMS570LC43x HDK. I just wanted to check flash download, so generated code from Halcogen, created empty project in CCS and later referenced the Halcogen source files. after successful code build, while trying to download I am getting the following load errors.
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR5: File Loader: Memory write failed: Unknown property "FlashBlankCheckToggle"
CortexR5: GEL: File: C:\Users\din2cob\ti example\example\Debug\example.out: Load failed.
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
I am getting the same error with both TI XDS100v2 and USB560v2 blackhawk system trace debugger
surprising that I am getting this error on my first attempt after unpacking the kit from the box.
please help