This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Preferred Emulator of Choice For Hercules?

Hello All,

I was wondering if you will share what your preferred emulator of choice is - I have the CCS and IAR tools - I tried using the SD XDS 200 with IAR for the 3137 HDK and had a lot of issues with it.  It seemed to work OK under CCS 6.x.  I also have the IAR JTAG i-Jet and and the JLink Lite - the Jet works great obviously under IAR; but it seems to work a *lot* better.  I had a problem getting the IAR/Segger JLink Lite to work at all under IAR.

So, a couple of questions:

With the Hercules Lock-Step (dog chasing fox) architecture; are there issues with certain emulators that are a little older maybe?  The Jet works so much better - and it is newer - so; just wanted to ask.

Do you need to set any special debug hooks or settings to make sure the emulator and debugger are stable with the development environment? (Other than the obvious settings.) Maybe an obvious question but wanted to ask.

There are no debug hooks exposed to the developer for the 'dog' core, is there?

Thanks,
John