Other Parts Discussed in Thread: TMS570LS1227, HALCOGEN
Dear TI,
In datasheet, it describes that TMS570LS1227 provides 1.6 DMIPS and has configurations which can run up to 180MHz providing up to 288 DMIPS. But when I benchmark it, the performance is just only 50 DMIPS. Could you explain it or solve it? Please refer my testing method.
I try 3 methods to benchmark _delay_cycles(1000) function, and measure their executed time.
1. Pin toggle
2. RTI
3. CCS(count event feature)
All of these 3 testing results are almost 50 DMIPS.
Please have the attached file.