This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are there any requirements on the device clock input related to the DCAN module? (CAN network timing related?)

Are there any requirements on the device clock input, (or tolerances on the crystal used with the device) related to the DCAN module?

  •  

    There is a detailed discussion of the DCAN oscillator timing in the TMS570LS Series Microcontroller Technical Reference Manual (TRM).

    (http://focus.ti.com/lit/ug/spnu489/spnu489.pdf)


    It’s in chapter 
    16.11.1.4 Oscillator Tolerance Range under the section that describes bit timing. 

    In summary, the DCAN module input clock/crystal tolerance(s) depend on the bit rate and network topology.  The TRM gives an example of a 125kbps, 40m network requiring a 1.58% tolerance. It would be good to plug in your own assumptions about bit timing and check against equations I and II in this section.