Hi all,
There is really very limited documentation about MibSPI TG interrupt setup. I could not find an example for this purpose.
1. How can I enable the system level interrupt?
2. How can I enable the MibSPI TG7 complete interrupt?
3. How can I link the TG7 complete interrupt to a ISR function?
It will be good to have an example of MibSPI interrupt. Thanks
Yuncheng
Some suggestions:
1. The technical reference for RM57x is really sub standard, there are numerous errors all over place.
2. In CCS 6.1 there is no way to restart the program as the restart button causing device disconnected.
3. The register name in technical reference does not match with the register name in CCS debug mode.