Hello,
This might seem like a foolish question, but is there a way to power the hercules rm42 launchpad with an external power supply. I have a 7.2V, 1500mA battery that I want to use to power the launchpad. I was thinking of connecting the the 5V pin on J3 column to the external battery through a voltage regulator (UA7805CKCT). I was just confused if this was viable because I wasn't sure if the pin was supposed to output or input 5V. So basically can I just connect the battery to a voltage regulator to the j3 5V pin, and it should power up and work?
Thank you,
Robert Lee