Hello.
I want to try hardware trace analyzer feature on TIVA microcontrollers. I use for this EK-TM4C123GXL launchpad and DK-TM4C129x development board.
When I tried to use Statistical Function Profiling in CodeComposerStudio 6.1, I've received a message "The specified breakpoint type "Trace" does not exist on this target".
I haven't find information about supporting Instrumentation Trace Module by Stellaris In-Circuid Debug Interface, which is implemented on specified development boards.
So, I have several questions now:
1. Is it possible to use trace analyzer on these boards whithout additional external emulator?
2. Can XDS200 perform this function for TIVA microcontrollers?
3. Which else emulators can be used for this purpose with TIVA microcontrollers?