Other Parts Discussed in Thread: HALCOGEN
Hi,
I have Recently bought the TMS570LS12x Launchpad, and when i am trying to Flash it with the built in example of SCI-UART9600, The Terminal is not showing anything i have checked every possible configuration. Even Bypassed The Code from Halcogen by configuring the Registers myself Still nothing on the Terminal.
Please help me through it, I want to see the output for this controller on the PC UART.
Also i have flashed the ADC example still nothing on the terminal. I have followed exact instructions from the HALCOGEN and flashed the example file.
Can I have a Tested Code for the Launch pad so that i can check it isnt a Hardware error/configuration error.
Thanks
Eeshan Bashir