This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SSI communication between eeprom and Tm4c123 controller



Hello sir,

I'm using the tiva tm4c123 launchpad. To read and write data from/into an Serial EEPROM  i'm using SSI communication. I have attached my program below. while reading an eeprom  i always got the value of 0x00 instead of the particular value that i  have written.  And I dont know that  where i did the mistake either in transmit part or receive part. I'm using 25c040 EEPROM

void  ssi_init()
{

SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralReset(SYSCTL_PERIPH_SSI0);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_5);//TX, CS, SCK are setted as output
GPIOPinTypeGPIOInput(GPIO_PORTA_BASE, GPIO_PIN_4);                                                   // RX is setted as input

//Pin Configuration

GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinConfigure(GPIO_PA5_SSI0TX);

GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5);
SSIClockSourceSet(SSI0_BASE, SSI_CLOCK_SYSTEM); // sets the system clock as the source of clock

SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 125000, 8);// defines base, System clk, Mode 0 = SPH = SPO = 0,Master, 125 KHz, no. of bits = 8 = 1 byte transfer

SSIEnable(SSI0_BASE); // enables SSI
}

 

void eeprom_write(unsigned int adr, unsigned char dat)
{
SysCtlDelay(100000);
GPIOPinWrite(GPIO_PORTA_BASE,CS,0xff);// Made the SS = 1
SysCtlDelay(100000);

GPIOPinWrite(GPIO_PORTA_BASE,CS,0x00); //Dropped down SS to select slave 25C040
SSIDataPut(SSI0_BASE,0x06);                            // sent the 0x06 as the required Write enable WREN command as per microchip Datasheet
while(SSIBusy(SSI0_BASE));                               //Wait until it transmit
GPIOPinWrite(GPIO_PORTA_BASE,CS,0xff);   // Pulsed high SS

SysCtlDelay(100000);
GPIOPinWrite(GPIO_PORTA_BASE,CS,0);      // pulled low SS for sending the remaining commands

SSIDataPut(SSI0_BASE,0x0A);                           // Cmd for Write cmd to SPI EEPROM as per datasheet

SSIDataPut(SSI0_BASE,adr);                              // Mem. location inside EEPROM
SSIDataPut(SSI0_BASE,dat);                              // test data
while(SSIBusy(SSI0_BASE));                              // wait till bzy
GPIOPinWrite(GPIO_PORTA_BASE,CS,0xff); // pulled high to complete write process

SysCtlDelay(1000000); // Twc
GPIOPinWrite(GPIO_PORTA_BASE, CS, 0);                               //CS = 0;
SSIDataPut(SSI0_BASE,0x02); while(SSIBusy(SSI0_BASE));//spi_WR(0x04);
GPIOPinWrite(GPIO_PORTA_BASE, CS, 8);                              //CS = 1;
SysCtlDelay(1000000);
}

unsigned char eeprom_read(unsigned int adr)
{
SysCtlDelay(100000);
GPIOPinWrite(GPIO_PORTA_BASE,GPIO_PIN_3,0xff);                // Made the SS = 1
SysCtlDelay(100000);


GPIOPinWrite(GPIO_PORTA_BASE, CS, 0);                                    //CS = 0;
SSIDataPut(SSI0_BASE,0x0B);                                                           // Cmd for read cmd to SPI EEPROM as per datasheet
SSIDataPut(SSI0_BASE, adr); while(SSIBusy(SSI0_BASE));       //Mem. location inside EEPROM
SSIDataGet(SSI0_BASE,reply);                                                          // Reading the memory location inside eeprom
GPIOPinWrite(GPIO_PORTA_BASE, CS, 8);                                   //CS = 1;

return(reply);                                                                                            //return the data present in ssi RX reg
}

void main()

{

//Enable the periphral...

ssi_init();             delay();// 100ms delay
eeprom_write(0,10);    delay();// 100ms delay

// here 0 is Address location in eeprom and 10 is data to be written

while(1)

{

unsigned char a=  eeprom_read(0);

display(a);

}}