Hello. We Have Rev E of TI Hercules Board RM48L952ZWT.
On HET1, we used all our "blackbox" PWMs on the NHETS (PWM0 to PWM7). How can we use extra NHET pins as PWMs? We cannot use the
void pwmSetSignal(hetRAMBASE_t * hetRAM, uint32 pwm, hetSIGNAL_t signal) HalCoGen function, because we have to pass PWM0 to PWM7 (not the HET pin number) and in HalCoGen is where we associate the pin# with the PWM. Is there another function that can have some unused pins generate pwm the way pwmSetSignal(hetRAMBASE_t * hetRAM, uint32 pwm, hetSIGNAL_t signal) allows us to do, but passing the unused pin numbers? Thank you.