This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC0 (channel-0) Interrupts configuration for desire analog threshold value of MCU TM4C123G



Hello Amit,

I am bit confuse asking for help, actually we want to setup or trigger analog ADC0 interrupt when input voltage more than its threshold limit( for e.g. 12V). It's really helpful, if you figure out the way of using API library of TM4C123G.

Platform : Keil/ MCU:TM4C123GH6Pxx /PLL : 50MHz

-Thanks in advance!