Other Parts Discussed in Thread: HALCOGEN
Hi everyone, I am doing an academy project about porting Autosar OS to TMS570. After reading papers and information about Autosar, Arctic Core and Arctic Studio, I have some questions:
1. I used to port FreeRTOS to TMS570 and it's very easy, I just included some *.h and *.c files of FreeRTOS, and then used the FreeRTOS functions to build my application on the chip. Can I do similarly to Autosar? If it is possible, which files should I include to my main.c
2. Second question, in FreeRTOS, I only need to use xcreatetask() function(this is a FreeRTOS function) to set task priority, and then i applied vstarttaskschedule() function to run the task in queue however I cannot see these kinds of functions in Autosar OS. Can someone tell me which function in autosar have same functionality like functions I said.
3. When I program Texas Instrument chips( TMS570 also), there is always main function which include the main program that we will build for the chip. However, I don't see any main functions in arctic Core example. How can the chips (TMS570, ...) runs our program without main function?
Please help me answer these questions!