This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 Silicon Revision



TMS570 Hercules Users,

 

There will be silicon revisions to the TMS570 Hercules product line to fix several critical issues.

  • TMS570LS21x/31x Rev C -> Rev D
  • TMS570LS11x/12x Rev B -> Rev C
  • TMS570LS03x/04x Rev A -> Rev B

 

The Part Change Notification (PCN) will be sent the end of June, 2015.  More detailed information on the change will be available at that time.

 

This post will provide the following information for TMS570 products.

  1. Which errata will be fixed in which product family.
  2. Schedule summary
  3. Impact of the fix.

 

Which errata will be fixed

The errata that will be fixed are listed in the first column of the table below.  There is a column for each TMS570 device family.  Meaning of “Fixed” is obvious.  N/A means the errata does not apply to that device family.  Errata that are listed in the errata sheet and not listed in this table will not be fixed.

 

Errata

TMS570LS21x / LS31x

TMS570LS11x / LS12x 

TMS570LS03x / LS04x

Power-on reset during bank 7 Sector erase may corrupt other sectors

(erratum DEVICE#B041)

N/A

N/A

Fixed

Reads of Bank7 may be corrupted by short glitches on nPORST pin

(erratum DEVICE#B042)

N/A

N/A

Fixed

Incorrect Write to External Memory using Store-Multiple CPU instruction

(erratum DEVICE#B064)

Fixed

Fixed

N/A

CPU write to peripheral or EMIF may be lost

(erratum DEVICE#B071)

Fixed

Fixed

N/A

PBIST ROM Algorithm Doesn’t Execute

(erratum PBIST#4)

Fixed

Fixed

Fixed

Change to PLL Lock Time

(erratum SWF021#44)

Fixed

Fixed

Fixed

 

Schedule Summary

The following table summarizes the schedule for the TMS570 product family.  Samples will be available as part of the PCN process.  Superset configurations of the device family will be available first followed by all P/Ns.  These schedules do not comprehend the EP products (for example TMS5703137-EP).

 

Milestone

TMS570LS21x / LS31x

TMS570LS11x / LS12x 

TMS570LS03x / LS04x

Development Samples

Now (TMS Rev C)

Now (TMS Rev B)

Now (TMS Rev A)

TMS release

Jun/15 (Rev D)

Jun/15 (Rev C)

Jun/15 (Rev B)

Production Samples

(<200units of superset P/Ns)

Jun/15 (Rev D)

SuperSet: TMS570LS3137

Jun/15 (Rev C)

SuperSet: TMS570LS1227

Jun/15 (Rev B)

SuperSet: TMS570LS0432

Production Samples (All P/Ns)

Sep/15 (Rev D)

Sep/15 (Rev C)

Sep/15 (Rev B)

Production Volume Shipments

Nov/15 (Rev D)

Nov/2015 (Rev C)

Nov/15 (Rev B)

 

The status of the safety certifications of the current revisions of the TMS570 production qualified devices are:

 

  • TMS570LS31x/21x rev C --> assessment complete; certificaton expected shortly
  • TMS570LS12x/11x rev B --> certified as of 11/2014
  • TMS570LS04x/03x rev A --> assessment starts this week, estimated early 3Q15 completion

 

The following updated devices are planned to go through functional safety assessment in 2015, following certifications of the current silicon.

 

  • TMS570LS31x/21x rev D --> estimated 4Q15 completion
  • TMS570LS12x/11x rev C --> estimated 3Q15 completion
  • TMS570LS04x/03x rev B --> estimated 4Q15 completion

 

Impact of the fix

The following table suggests what changes may be required for the new revisions. 

 

Errata

Change required for new revisions

Power-on reset during bank 7 Sector erase may corrupt other sectors

(erratum DEVICE#B041)

May leave workaround in place, no change to SW required

Reads of Bank7 may be corrupted by short glitches on nPORST pin

(erratum DEVICE#B042)

May leave workaround in place, no change to SW required

Incorrect Write to External Memory using Store-Multiple CPU instruction

(erratum DEVICE#B064)

May leave workaround in place, no change to SW required

Change can be made to re-gain EMIF performance

CPU write to peripheral or EMIF may be lost

(erratum DEVICE#B071)

May leave workaround in place, no change to SW required

PBIST ROM Algorithm Doesn’t Execute

(erratum PBIST#4)

May leave workaround in place, no change to SW required

Change to PLL Lock Time

(erratum SWF021#44)

Evaluate impact of additional 384 OSCIN cycles

 

TI does not anticipate the changes made in revised devices to impact estimated safety metrics in the device safety analysis reports nor recommendations made in device safety manuals. The customer is responsible for evaluating all functional safety related impact, if any, of these changes to the implemented system and to take appropriate actions to mitigate any perceived impact to system level functional safety.

 

Regards,

Dave

 

 

  • Hi Dave

    "These schedules do not comprehend the EP products... "
    Could you please list the revision schedule for the TMS5703137-EP version?

    Best regards
    Ove Toft
  • Ove,

    Unfortunately, that is another TI group that specializes in extended operation.  

    I'll ask them to post to this thread.

    Regards,
    Dave

  • TMS570 Hercules Users,

     There has been a delay in schedule.

     There will be silicon revisions to the TMS570 Hercules product line to fix several critical issues.

    • TMS570LS21x/31x Rev C -> Rev D
    • TMS570LS11x/12x Rev B -> Rev C
    • TMS570LS03x/04x Rev A -> Rev B

     The Part Change Notification (PCN) will be sent the end of July, 2015.  More detailed information on the change will be available at that time.

     Schedule Summary

    The following table summarizes the schedule for the TMS570 product family.  Samples will be available as part of the PCN process.  Superset configurations of the device family will be available first followed by all P/Ns.  These schedules do not comprehend the EP products (for example TMS5703137-EP).

     

    Milestone

    TMS570LS21x / LS31x

    TMS570LS11x / LS12x 

    TMS570LS03x / LS04x

    Development Samples

    Now (TMS Rev C)

    Now (TMS Rev B)

    Now (TMS Rev A)

    TMS release

    Jul/15 (Rev D)

    Jul/15 (Rev C)

    Aug/15 (Rev B)

    Production Samples

    (<200units of superset P/Ns)

    Jul/15 (Rev D)

    SuperSet: TMS570LS3137

    Jul/15 (Rev C)

    SuperSet: TMS570LS1227

    Aug/15 (Rev B)

    SuperSet: TMS570LS0432

    Production Samples (All P/Ns)

    Oct/15 (Rev D)

    Oct/15 (Rev C)

    Nov/15 (Rev B)

    Production Volume Shipments

    Dec/15 (Rev D)

    Dec/2015 (Rev C)

    Jan/16 (Rev B)

     The status of the safety certifications of the current revisions of the TMS570 production qualified devices are: 

    • TMS570LS31x/21x rev C --> assessment complete; certificaton expected shortly
    • TMS570LS12x/11x rev B --> certified as of 11/2014
    • TMS570LS04x/03x rev A --> estimated early 3Q15 completion 

    The following updated devices are planned to go through functional safety assessment in 2015, following certifications of the current silicon. 

    • TMS570LS31x/21x rev D --> estimated 4Q15 completion
    • TMS570LS12x/11x rev C --> estimated 3Q15 completion
    • TMS570LS04x/03x rev B --> estimated 1Q16 completion 

    Regards,

    Dave