Hi,
I am trying to use the gpio pin to drive led using the uln2803.I have set the gpio drive strength to 12 ma.Even after using 2 pins to drive led I am not able to drive the led using tiva c connected Launchpad gpio.where as I am able to drive the led from external powersource set at 10 ma current output.Is there a problem in the way I am interfacing uln2803 can help me with this.
Regards
Manoj